HTTP post

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

HTTP post

2,024 次查看
Swapnil_Enable
Contributor III

Hi i am trying to POST data to Google spreadsheet like andrino, but i am not able succeed. i have return the code for POST.

strcat (cServer_WriteBuff,"entry.1446189103=");
strcat (cServer_WriteBuff,POST);
strcat (cServer_WriteBuff,"&submit=Submit");
value = strlen(cServer_WriteBuff);
error = send(sock, "POST /formResponse?formkey=", sizeof("POST /formResponse?formkey="), 0);
error = send(sock, (void *)formkey, sizeof(formkey), 0);
error = send(sock, "&ifq HTTP/1.1\r\n", sizeof("&ifq HTTP/1.1\r\n"), 0);
error = send(sock, "Host: spreadsheets.google.com\r\n", sizeof("Host: spreadsheets.google.com\r\n"), 0);
error = send(sock, "Content-Type: application/x-www-form-urlencoded\r\n", sizeof("Content-Type: application/x-www-form-urlencoded\r\n"), 0);
error = send(sock, "Connection: close\r\n", sizeof("Connection: close\r\n"), 0);
error = send(sock, (void *)value, sizeof(value), 0);
error = send(sock, "\r\n", sizeof("\r\n"), 0);
error = send(sock, "\r\n", sizeof("\r\n"), 0);
error = send(sock, (void *)cServer_WriteBuff, sizeof(cServer_WriteBuff), 0);
error = send(sock, "\r\n", sizeof("\r\n"), 0);
error = send(sock, "\r\n", sizeof("\r\n"), 0);

  but when i check it on Hercules terminal, it only shows " POST /formResponse?formkey=" can anyone please help to figure out, or any suggestion. i am tring to use httpsrv code but being a beginner not able to figure how to use it.

标签 (1)
标记 (1)
0 项奖励
回复
1 回复

1,545 次查看
karelm_
Contributor IV

Hi,

please try to use function strlen instead of sizeof in calls of send() function. Using sizeof in this context means that you also send terminating null character ('\0') in your messages, which is probably why you cannot receive any other than first message. Also on line 16 you are calling sizeof(formkey). I assume, that variable formkey is pointer so sizeof will return 4, which is probably not what you want. If you want to get length of string formkey is pointing to you should use strlen(formkey).

Best regards

Karel

0 项奖励
回复