HTTP client into MQX?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

HTTP client into MQX?

Jump to solution
7,769 Views
arnogir
Senior Contributor II

Hello

 

To upgrade and add some function to an existing product, I would know if with MQX 4.2 (on a Kinetis K70) we can use an HTTP Client?

 

The aim for us is to send a couple of data to a HTTp server.

 

Regards,

 

 

0 Kudos
Reply
1 Solution
7,739 Views
danielchen
NXP TechSupport
NXP TechSupport

Hi @arnogir :

 

Please refer to attached zip file.

 

Regards

Daniel

View solution in original post

0 Kudos
Reply
7 Replies
7,693 Views
arnogir
Senior Contributor II

Hello,

 

In the same way, if MQX can integrate a FTP client? (To send file to a distant FTP server)?

Is there an exemple?

Thank

0 Kudos
Reply
7,763 Views
danielchen
NXP TechSupport
NXP TechSupport

Hi

 

I would suggest you refer to AN4417.  It demonstrated http client implementation using MQX RTOS capabilities. The hardware used to illustrate this is the TWR-K60N512.

 

 

Regards

Daniel

0 Kudos
Reply
7,756 Views
arnogir
Senior Contributor II

Thank a lot.

 

Could you indicate me where can I find the .zip which contains file exemple?

Are link from "Frescale" are broken.

 

Thank

0 Kudos
Reply
7,740 Views
danielchen
NXP TechSupport
NXP TechSupport

Hi @arnogir :

 

Please refer to attached zip file.

 

Regards

Daniel

0 Kudos
Reply
7,732 Views
arnogir
Senior Contributor II

Thank a lot

 

Regards

0 Kudos
Reply
7,577 Views
arnogir
Senior Contributor II

Hello

In the same way, is the HTTPS is possible?

 

Regards

0 Kudos
Reply
7,753 Views
danielchen
NXP TechSupport
NXP TechSupport

Yes, the link is broken.  I can not get it neither.

I will update you if I get it.

 

Regards

Daniel

0 Kudos
Reply