HTTP client into MQX?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

HTTP client into MQX?

ソリューションへジャンプ
7,891件の閲覧回数
arnogir
Senior Contributor II

Hello

 

To upgrade and add some function to an existing product, I would know if with MQX 4.2 (on a Kinetis K70) we can use an HTTP Client?

 

The aim for us is to send a couple of data to a HTTp server.

 

Regards,

 

 

0 件の賞賛
返信
1 解決策
7,861件の閲覧回数
danielchen
NXP TechSupport
NXP TechSupport

Hi @arnogir :

 

Please refer to attached zip file.

 

Regards

Daniel

元の投稿で解決策を見る

0 件の賞賛
返信
7 返答(返信)
7,815件の閲覧回数
arnogir
Senior Contributor II

Hello,

 

In the same way, if MQX can integrate a FTP client? (To send file to a distant FTP server)?

Is there an exemple?

Thank

0 件の賞賛
返信
7,885件の閲覧回数
danielchen
NXP TechSupport
NXP TechSupport

Hi

 

I would suggest you refer to AN4417.  It demonstrated http client implementation using MQX RTOS capabilities. The hardware used to illustrate this is the TWR-K60N512.

 

 

Regards

Daniel

0 件の賞賛
返信
7,878件の閲覧回数
arnogir
Senior Contributor II

Thank a lot.

 

Could you indicate me where can I find the .zip which contains file exemple?

Are link from "Frescale" are broken.

 

Thank

0 件の賞賛
返信
7,862件の閲覧回数
danielchen
NXP TechSupport
NXP TechSupport

Hi @arnogir :

 

Please refer to attached zip file.

 

Regards

Daniel

0 件の賞賛
返信
7,854件の閲覧回数
arnogir
Senior Contributor II

Thank a lot

 

Regards

0 件の賞賛
返信
7,699件の閲覧回数
arnogir
Senior Contributor II

Hello

In the same way, is the HTTPS is possible?

 

Regards

0 件の賞賛
返信
7,875件の閲覧回数
danielchen
NXP TechSupport
NXP TechSupport

Yes, the link is broken.  I can not get it neither.

I will update you if I get it.

 

Regards

Daniel

0 件の賞賛
返信