Generating a frequency

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

Generating a frequency

跳至解决方案
4,803 次查看
Jairo
Contributor III

Hi i want to know if there's somebody who can help me with this, i need to generate a pulse signal in one pin (20 MHz). First of all i was able to do so but at very low frequencies compared with this, to achieve it i modified the timer example program to toggle the state of a pin. Another attempt i made was to copy the configuration made from Processor Expert and adapt it to MQX but with unsatisfactory results.

 

 /************************** 20MHz USING GPT**************************************/ //*********************************************************************************************    printf("Inicializando frecuencia...");    clrReg8Bits(reg_ptr->GPT.GPTIE, 0x02);  //Disable interrupts    setReg8(reg_ptr->GPT.GPTSCR1, 0x00);    //Stop Timer    setReg8Bits(reg_ptr->GPT.GPTIOS, 0x0A);     clrSetReg8Bits(reg_ptr->GPT.GPTCTL1, 0xC8, 0x04);        clrReg8Bits(reg_ptr->GPT.GPTCTL2, 0xCC);               setReg8(reg_ptr->GPT.GPTSCR2,0x08);    setReg16(reg_ptr->GPT.GPTC1, 0x01U);    //Store the given number in the compare registry    setReg16(reg_ptr->GPT.GPTC3, 0x01U);    //                    setReg8Bit(reg_ptr->GPT.GPTSCR1 , 0x80U); //Run the timer

Regarding all my attempts i got some doubts with MQX

1. In time what is a tick?

2. Is there another way to toggle on/off a pin, or i got to use the ioctl functions?

3. Which is the minimum intervalusing the lwtimer instead the timer?

 

Thanks in advance.

 

0 项奖励
回复
1 解答
3,316 次查看
DavidS
NXP Employee
NXP Employee

Hi Jairo,

I wouldn't recommend bit banging method for high frequency clock generation.   I'd setup a DMA Timer to toggle its output pin when it reaches a particular value.  It then can reset the counter and repeat the process without any processor/CPU intervention.  You can also update the reference count value to change the frequency/clock output.

The "tick" in the RTOS is 5ms.

Regards,

David 

在原帖中查看解决方案

0 项奖励
回复
5 回复数
3,316 次查看
ipa
Contributor III

Hi Jairo,

Did you looked at PWM module? it is capable of clock up to Internal_Bus_Clock/2.

I did not make any further checks on setting the rest of PWM ...

Another solution is to use CLKOUT and dividing externally by 4 if you run at 80MHz.

Regards,

IPA 

0 项奖励
回复
3,317 次查看
DavidS
NXP Employee
NXP Employee

Hi Jairo,

I wouldn't recommend bit banging method for high frequency clock generation.   I'd setup a DMA Timer to toggle its output pin when it reaches a particular value.  It then can reset the counter and repeat the process without any processor/CPU intervention.  You can also update the reference count value to change the frequency/clock output.

The "tick" in the RTOS is 5ms.

Regards,

David 

0 项奖励
回复
3,316 次查看
CarlFST60L
Senior Contributor II

We were considering making a 512Khz square wave output with another signal doing a single pulse every 16 counts (Generating PCM and Sync). Would this be possible without adding load to the processor?(Our processor is already pushing very high speed SPI and 3 UARTS among other hi load threads.

 

I know in the 8 bit processors it would be easy as they have a timer and modulo counter which you can easily setup and leave runing with zero processor loading as the module just toggles when the counter reachs module.

 

0 项奖励
回复
3,316 次查看
Jairo
Contributor III

Thnks to all for your replies, i've decided to generate the frequncy using the DMA Timer instead the PWM because the signal is 50% duty cycle, so i use the flip-flop function in the timer.

 

Best Regards.

0 项奖励
回复
3,316 次查看
CarlFST60L
Senior Contributor II
Can someone post an example of using the DMA timer to generate a PWM? Or is there an example somewhere?
0 项奖励
回复