GPIO simple output with kinetis kwikstik

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

GPIO simple output with kinetis kwikstik

ソリューションへジャンプ
3,510件の閲覧回数
alexdev83
Contributor II

Hi, I'm trying to write a simple program for make blinking a led linked on GPIO pin 6 of my Kwikstik (with the TWR-ELEV).

 

I'm working with Codewarrior 10.1 (with the lastest update patch) and MQX 3.7 + KwikStik Patch.

 

This the code I have wrote. The codewarrior compile without errors but it not work..

 

#include "main.h"

#include <io_gpio.h>
#include <io_gpio_kgpio.h>




#if !BSPCFG_ENABLE_IO_SUBSYSTEM
#error This application requires BSPCFG_ENABLE_IO_SUBSYSTEM defined non-zero in user_config.h. Please recompile BSP with this option.
#endif


#ifndef BSP_DEFAULT_IO_CHANNEL_DEFINED
#error This application requires BSP_DEFAULT_IO_CHANNEL to be not NULL. Please set corresponding BSPCFG_ENABLE_TTYx to non-zero in user_config.h and recompile BSP with this option.
#endif


TASK_TEMPLATE_STRUCT MQX_template_list[] =
{
/*  Task number, Entry point, Stack, Pri, String, Auto? */
   {MAIN_TASK,   Main_task,   1500,  9,   "main", MQX_AUTO_START_TASK},
   {0,           0,           0,     0,   0,      0,                 }
};

GPIO_PIN_STRUCT pins1[] = {
        
    GPIO_PORT_A | GPIO_PIN6,
    GPIO_LIST_END
};
/*TASK*-----------------------------------------------------
*
* Task Name    : Main_task
* Comments     :
*    This task prints " Hello World "
*
*END*-----------------------------------------------------*/

void Main_task(uint_32 initial_data)
{
    MQX_FILE_PTR file1;

    
   _io_gpio_install("gpio:");
   
   file1 = fopen("gpio:write", (char_ptr) &pins1);
   
   


while (1) {

     
       _io_ioctl(file1, GPIO_IOCTL_WRITE_LOG1, NULL);
       
       _time_delay(1000);
       
       _io_ioctl(file1, GPIO_IOCTL_WRITE_LOG0 NULL);
       
       _time_delay(1000);
}   
   //_mqx_exit(0);


/* EOF */

-------------------------------------------------------------------------------------------------------------------------------------------

 

I have already set to one GPIO in userconfig.h

 

Someone find errors in this code?

 

Thanks

 

0 件の賞賛
返信
1 解決策
2,646件の閲覧回数
alexdev83
Contributor II

I have resolved my problem!

The mistake that I commit is that I confuse Name and Usage of Tower Elevator Connections in Kwikstik Manual!!

Thanks however for your responses!
 

元の投稿で解決策を見る

0 件の賞賛
返信
10 返答(返信)
2,646件の閲覧回数
c0170
Senior Contributor III

HI,

 

There are no LEDs you can blink on kwikstik. I assume you connected your own LED to PTA6 pin.

Also you should check return values if file is opened and you write logical values to the pin.

 

Start with LWGPIO which is much easier to use.

 

Regards,

MartinK

0 件の賞賛
返信
2,645件の閲覧回数
alexdev83
Contributor II

Thanks for your response, I have tried with LWGPIO, but the result is the same.

 

This is my code (I want only turn on a led connected on GPIO6, in the side A expansion port of the tower):

--------------------------------------------------------------------------------------------------------------------------

#include <mqx.h>
#include <bsp.h>
#include <lwgpio.h>
#include <lwgpio_kgpio.h>


 

void main_task
   (
      uint_32 initial_data
   )
{
    
    boolean status;
    LWGPIO_STRUCT led1;
    
    status = lwgpio_init(&led1, LWGPIO_PORT_A | LWGPIO_PIN6, LWGPIO_DIR_OUTPUT, LWGPIO_VALUE_HIGH);
    if (status != TRUE) {
        printf("LWGPIO FAIL.\n");

    }
    else
    {
        printf("LWGPIO OK.\n");

    }
    
    while (TRUE);

    };
/* EOF */
}

-------------------------------------------------------------------------------------------------------------------------------------------------

I also tried this:

 

status = lwgpio_init(&led1, LWGPIO_PIN6, LWGPIO_DIR_OUTPUT, LWGPIO_VALUE_HIGH);

 

in the codewarrior console i see "LWGPIO OK" but the led don't turn on...

 

Do you see errors in my code?

Or the problem are the power connection on the tower? (I Have the Kwikstik connected the to PC with USB cable in Jlink connector and the twr-elev connected to the pc with USB cable in S4 connector and SW1 switch turned on)

 

 

 

0 件の賞賛
返信
2,646件の閲覧回数
MarkP_
Contributor V

Hi,

you need also set the io-pin mode by function lwgpio_set_functionality().

Example:

lwgpio_set_functionality(&led1, LWGPIO_MUX_PTA6_GPIO);

~Mark

 

0 件の賞賛
返信
2,646件の閲覧回数
alexdev83
Contributor II

I modified the code:

----------------------------------------------------------------------------------------------------------------------------------------------------------------

void main_task
   (
      uint_32 initial_data
   )
{
    LWGPIO_STRUCT led1;
    boolean status;
      
        
        status = lwgpio_init(&led1, LWGPIO_PORT_A | LWGPIO_PIN7, LWGPIO_DIR_OUTPUT, LWGPIO_VALUE_HIGH);
        if (status != TRUE) {
            printf("LWGPIO FAIL.\n");

        }
        else
        {
            printf("LWGPIO OK.\n");

        }
        
        lwgpio_set_functionality(&led1, LWGPIO_MUX_A7_GPIO);
        lwgpio_set_value(&led1, LWGPIO_VALUE_HIGH);
        
        while (TRUE){
            //test

        }


}

------------------------------------------------------------------------------------------------------

but the problem is the same. (If I make the debug,   lwgpio_set_functionality and lwgpio_set_value returns a non zero value)

0 件の賞賛
返信
2,646件の閲覧回数
c0170
Senior Contributor III

Hello alexdev83,

 

why did you connect LED to PTA7 ? That pin is for Microphone signal (schematic for kwikstik, page9). Try another pin.

 

I run an example where i toogled GPIO_PORT_A | GPIO_PIN12.

 

Regards,

MartinK

0 件の賞賛
返信
2,646件の閲覧回数
alexdev83
Contributor II
Sorry, but in kwikstik manual i don't see gpio pin12. Where is connected?
0 件の賞賛
返信
2,646件の閲覧回数
c0170
Senior Contributor III
0 件の賞賛
返信
2,646件の閲覧回数
alexdev83
Contributor II

I saw the scheme you indicate. But i haven't a connector for link the led to the TWRPI SOCKETS.

 

Can you say me where I can link the led in the A Side expansion port of the TWR-ELEV and a simple code for make power on the led?

 

 

Thanks

0 件の賞賛
返信
2,646件の閲覧回数
alexdev83
Contributor II

(The schematics that you linked to me is relative to TWR-K40X256, not to Kwikstik I have!!!!)

0 件の賞賛
返信
2,647件の閲覧回数
alexdev83
Contributor II

I have resolved my problem!

The mistake that I commit is that I confuse Name and Usage of Tower Elevator Connections in Kwikstik Manual!!

Thanks however for your responses!
 

0 件の賞賛
返信