GPIO Example so simple I can not see why it does not work

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

GPIO Example so simple I can not see why it does not work

Jump to solution
4,278 Views
w2vy
Contributor V

This example is so simple I can not see why it does not work!

It just loops reading a pin table from gpio:read and extracts the values and prints them.

They all come up as 1

 

any ideas?

 

I am running MQX 3.6 on a mcf52259demo board.

I have the gpio pins wired on J4 so I can pull the up/down and watch for changes

 

Code below... (and attached if you want to compile)

 

tom

 

/*TASK*-----------------------------------------------------------------** Function Name  : Main_task* Comments       :*    This task initializes RTCS and starts SHELL.**END------------------------------------------------------------------*/TASK_TEMPLATE_STRUCT MQX_template_list[] ={/*  Task number, Entry point, Stack, Pri, String, Auto? */   {MAIN_TASK,   Main_task,   3000,  9,   "main",        MQX_AUTO_START_TASK, 0, 50},   {0,           0,           0,     0,   0,             0, 0, 0}};#define GPIO_W1  GPIO_PORT_TA | GPIO_PIN3#define GPIO_W0  GPIO_PORT_TA | GPIO_PIN2#define GPIO_H1  GPIO_PORT_TA | GPIO_PIN1#define GPIO_H0  GPIO_PORT_TA | GPIO_PIN0#define GPIO_D7  GPIO_PORT_AN | GPIO_PIN7#define GPIO_D6  GPIO_PORT_AN | GPIO_PIN6#define GPIO_D5  GPIO_PORT_AN | GPIO_PIN5#define GPIO_D4  GPIO_PORT_AN | GPIO_PIN4#define GPIO_D3  GPIO_PORT_AN | GPIO_PIN3#define GPIO_D2  GPIO_PORT_AN | GPIO_PIN2#define GPIO_D1  GPIO_PORT_AN | GPIO_PIN1#define GPIO_D0  GPIO_PORT_AN | GPIO_PIN0#define GPIO_J16 GPIO_PORT_TC | GPIO_PIN2#define GPIO_J17 GPIO_PORT_TC | GPIO_PIN1#define GPIO_FLIP  GPIO_PORT_UC | GPIO_PIN3#define GPIO_RESET GPIO_PORT_TC | GPIO_PIN3#define GPIO_SYNC  GPIO_PORT_NQ | GPIO_PIN1MQX_FILE_PTR inputfd;static GPIO_PIN_STRUCT pins_input[] = {   GPIO_W1,   GPIO_W0,   GPIO_H1,   GPIO_H0,   GPIO_D7,   GPIO_D6,   GPIO_D5,   GPIO_D4,   GPIO_D3,   GPIO_D2,   GPIO_D1,   GPIO_D0,   GPIO_J16,   GPIO_J17,   GPIO_LIST_END};int bin_pins(GPIO_PIN_STRUCT pins[], int bits);void Main_task(uint_32 initial_data){   int w, h, J16, J17;   volatile MCF5225_STRUCT _PTR_ reg_ptr = _PSP_GET_IPSBAR();   volatile MCF5225_GPIO_STRUCT _PTR_ gpio = &reg_ptr->GPIO;   // TA0-3 Inputs   inputfd = fopen("gpio:input", (char *)&pins_input);   if (inputfd == NULL) {      printf("Error opening GPIO Files!\r\n");      _task_block();   }   printf("GPIO Opened ok\r\n");   while (1) {      w = h = 1;      if (ioctl(inputfd, GPIO_IOCTL_READ, &pins_input) == IO_OK) {         w = bin_pins(&pins_input[0], 2) + 1;         h = bin_pins(&pins_input[2], 2) + 1;         J16 = bin_pins(&pins_input[12], 1);         J17 = bin_pins(&pins_input[13], 1);      }      printf("H %d W %d J16 %d J17 %d PORTTA %x DDR %x PAR %x PORTTAP %x\r\n", h, w, J16, J17, gpio->PORTTA, gpio->DDRTA, gpio->PTAPAR, gpio->PORTTAP_SETTA);      _time_delay(1000);   }}

 

 

0 Kudos
Reply
1 Solution
2,610 Views
JuroV
NXP Employee
NXP Employee

In fact, your GPIO IP on the chip reads "1" from input. So the problem must be in the electrical connection.

View solution in original post

0 Kudos
Reply
5 Replies
2,610 Views
w2vy
Contributor V

BTW The printf generates the following output

 

H 4 W 4 J16 1 J17 1 PORTTA f DDR 0 PAR 0 PORTTAP fH 4 W 4 J16 1 J17 1 PORTTA f DDR 0 PAR 0 PORTTAP fH 4 W 4 J16 1 J17 1 PORTTA f DDR 0 PAR 0 PORTTAP fH 4 W 4 J16 1 J17 1 PORTTA f DDR 0 PAR 0 PORTTAP f

 

DDR 0 = Outputs, PARTA = 0 GPIO, Output reg F and Pin (PORTTAP) F

 

sigh

 

I sure hope it is stupid... those are easy to fix :smileyhappy:

0 Kudos
Reply
2,610 Views
JuroV
NXP Employee
NXP Employee

I dont understand, Is your example already working?

If not, what does you bin_pins function do?

At the end:

DDR = 0 => inputs

 

0 Kudos
Reply
2,610 Views
w2vy
Contributor V

bin_pins just extracts bits from the pin table.

 

All the pins read as 1

 

when when I have the pins pulled low

 

tom

0 Kudos
Reply
2,611 Views
JuroV
NXP Employee
NXP Employee

In fact, your GPIO IP on the chip reads "1" from input. So the problem must be in the electrical connection.

0 Kudos
Reply
2,610 Views
w2vy
Contributor V

(blush)

 

It turns out the pin on J4 that I was using to pull down the other ones, was not ground.

 

Well it was a simple solution!

 

Thanks for the public embarassment!

I guess that is the price we pay for asking for help publically!

 

:smileyhappy:

0 Kudos
Reply