Flexbus read and write issue in MQX

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Flexbus read and write issue in MQX

1,007 Views
daweiyou
NXP Employee
NXP Employee

Hi:

 

I follow Flexbus demo case in MQX to write CAN application,

compared with original demo, I use mulitple mailbox for read/write.

But this application only can TX or RX, for example: one node run TX task, another run RX task, which is OK.

But the node run RX and TX togrther, which couldn't run well, it couldn't receive corrent data from another node, even can't enter into ISR.

the code run two nodes is same, only node ID is different.

So please help check attached file, thx!

Original Attachment has been moved to: test.h.zip

Original Attachment has been moved to: fc.c.zip

0 Kudos
Reply
1 Reply

856 Views
danielchen
NXP TechSupport
NXP TechSupport

Hi Dawei:

which board you are using, K60F120 or K70F120 ?


Daniel

0 Kudos
Reply