Flexbus read and write issue in MQX

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Flexbus read and write issue in MQX

1,003件の閲覧回数
daweiyou
NXP Employee
NXP Employee

Hi:

 

I follow Flexbus demo case in MQX to write CAN application,

compared with original demo, I use mulitple mailbox for read/write.

But this application only can TX or RX, for example: one node run TX task, another run RX task, which is OK.

But the node run RX and TX togrther, which couldn't run well, it couldn't receive corrent data from another node, even can't enter into ISR.

the code run two nodes is same, only node ID is different.

So please help check attached file, thx!

Original Attachment has been moved to: test.h.zip

Original Attachment has been moved to: fc.c.zip

0 件の賞賛
返信
1 返信

852件の閲覧回数
danielchen
NXP TechSupport
NXP TechSupport

Hi Dawei:

which board you are using, K60F120 or K70F120 ?


Daniel

0 件の賞賛
返信