Flexbus doesn't work!

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Flexbus doesn't work!

1,909件の閲覧回数
amleng
Contributor IV

Hello Freescale,

 

I try to run the sample code explained in AN4393 (section 3.1.2)

on TWR-K60F120M and TWR-MEM. In my code I write and read

an 8-bit value in the first 16 location of MRAM. The interesting is

that once I disconnect the twr-mem from the cpu, it still write and

read the right value. To me that means the value is written in

internal ram not external! I attach my MQX 4.0.2 project created

by CW 10.5 to this email.

 

I wonder if I need to change something in BSP or user config to

enable the external memory?!

 

Cheers

Original Attachment has been moved to: flexbus.rar

0 件の賞賛
返信
2 返答(返信)

1,615件の閲覧回数
Martin_
NXP Employee
NXP Employee

Note the AN4393 uses 0x60000000 as base address for Flexbus. On K60F120M it is cacheable memory region. After you disconnect TWR-MEM you should invalidate the cache line to force the MCU to access physical memory.  MQX provides: void _dcache_invalidate_line(void *addr) function for this.

It is also possible to use 0xA0000000 for Flexbus non-cacheable access.

0 件の賞賛
返信

1,615件の閲覧回数
amleng
Contributor IV

Hello Martin,

Thank you for your reply. That was very helpul. I used 0xA0000000 as the base address and that works well on the TWR-MEM.

So, I try to implement the same concept on a customized board with a 16bit SRAM. The figure below shows our hardware schematic.

Flexbus.png

The memory is word-addressable (16-bit), so the FlexBus word address line FB_AD[1] is connected to A[0] of the memory.

Thus, FB_A[15:1] are connected to A[14:0] of the memory.

I initialize the flex bus in 16bit mode using the following code:

#define FLEX_BASE_ADDRESS 0xA0000000

SIM_SCGC7 |= SIM_SCGC7_FLEXBUS_MASK; // Enable the clock to the FlexBus

SIM_CLKDIV1 |= SIM_CLKDIV1_OUTDIV3(0x0); //FlexBus Clock not divided

// Set the GPIO ports clocks

SIM_SCGC5 = SIM_SCGC5_PORTA_MASK | SIM_SCGC5_PORTB_MASK | SIM_SCGC5_PORTC_MASK |

SIM_SCGC5_PORTD_MASK | SIM_SCGC5_PORTE_MASK;

// Set the GPIO ports clocks

SIM_SCGC5 = SIM_SCGC5_PORTA_MASK | SIM_SCGC5_PORTB_MASK | SIM_SCGC5_PORTC_MASK |

SIM_SCGC5_PORTD_MASK | SIM_SCGC5_PORTE_MASK;

/*address bus*/

PORTB_PCR18 = PORT_PCR_MUX(5); // fb_ad[15]

PORTC_PCR0 = PORT_PCR_MUX(5); // fb_ad[14]

PORTC_PCR1 = PORT_PCR_MUX(5); // fb_ad[13]

PORTC_PCR2 = PORT_PCR_MUX(5); // fb_ad[12]

PORTC_PCR4 = PORT_PCR_MUX(5); // fb_ad[11]

PORTC_PCR5 = PORT_PCR_MUX(5); // fb_ad[10]

PORTC_PCR6 = PORT_PCR_MUX(5); // fb_ad[9]

PORTC_PCR7 = PORT_PCR_MUX(5); // fb_ad[8]

PORTC_PCR8 = PORT_PCR_MUX(5); // fb_ad[7]

PORTC_PCR9 = PORT_PCR_MUX(5); // fb_ad[6]

PORTC_PCR10 = PORT_PCR_MUX(5); // fb_ad[5]

PORTD_PCR2 = PORT_PCR_MUX(5); // fb_ad[4]

PORTD_PCR3 = PORT_PCR_MUX(5); // fb_ad[3]

PORTD_PCR4 = PORT_PCR_MUX(5); // fb_ad[2]

PORTD_PCR5 = PORT_PCR_MUX(5); // fb_ad[1]

PORTD_PCR6 = PORT_PCR_MUX(5); // fb_ad[0]

/*data bus*/

PORTB_PCR20 = PORT_PCR_MUX(5); // fb_ad[31] used as d[15]

PORTB_PCR21 = PORT_PCR_MUX(5); // fb_ad[30] used as d[14]

PORTB_PCR22 = PORT_PCR_MUX(5); // fb_ad[29] used as d[13]

PORTB_PCR23 = PORT_PCR_MUX(5); // fb_ad[28] used as d[12]

PORTC_PCR12 = PORT_PCR_MUX(5); // fb_ad[27] used as d[11]

PORTC_PCR13 = PORT_PCR_MUX(5); // fb_ad[26] used as d[10]

PORTC_PCR14 = PORT_PCR_MUX(5); // fb_ad[25] used as d[9]

PORTC_PCR15 = PORT_PCR_MUX(5); // fb_ad[24] used as d[8]

PORTB_PCR6 = PORT_PCR_MUX(5); // fb_ad[23] used as d[7]

PORTB_PCR7 = PORT_PCR_MUX(5); // fb_ad[22] used as d[6]

PORTB_PCR8 = PORT_PCR_MUX(5); // fb_ad[21] used as d[5]

PORTB_PCR9 = PORT_PCR_MUX(5); // fb_ad[20] used as d[4]

PORTB_PCR10 = PORT_PCR_MUX(5); // fb_ad[19] used as d[3]

PORTB_PCR11 = PORT_PCR_MUX(5); // fb_ad[18] used as d[2]

PORTB_PCR16 = PORT_PCR_MUX(5); // fb_ad[17] used as d[1]

PORTB_PCR17 = PORT_PCR_MUX(5); // fb_ad[16] used as d[0]

PORTB_PCR19 = PORT_PCR_MUX(5); // fb_oe_b

PORTC_PCR11 = PORT_PCR_MUX(5); // fb_rw_b

PORTD_PCR1 = PORT_PCR_MUX(5); // fb_cs0_b

PORTD_PCR0 = PORT_PCR_MUX(5); // fb_ale

FB_CSAR0 = (unsigned int)&MRAM_START_ADDRESS_8; //Set Base address

FB_CSCR0 = FB_CSCR_PS(2) // 16-bit port

| FB_CSCR_AA_MASK // auto-acknowledge

| FB_CSCR_WS(0x2) // 2 wait states

;

FB_CSMR0 = FB_CSMR_BAM(0x7) //Set base address mask for 512K address space

| FB_CSMR_V_MASK //Enable cs valid signal

;

I try to write and read a 16bit value to the SRAM over flexbus by using the following code:

int wdata16 = 1;

unsigned short *p_16;

p_16 = (unsigned short*) FLEX_BASE_ADDRESS;

for(n=0x00010;n<0x001F;n++) //address offset

{

    *(p_16 + n) = wdata16;

     rdata16 = *(p_16 + n);

     wdata16<<=1;

}

the problem is that rdata value is different from wdata! I'm not sure if I missed something in hardware or firmware side!

any comment on this issue kindly appreciated.

Cheer!

0 件の賞賛
返信