File > New > MQX4.2 project missing from codewarrior

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

File > New > MQX4.2 project missing from codewarrior

1,127 Views
carlnormansuret
Contributor V

I have installed MQX4.1 and MQX4.2 on CW10.7 pro and need to run some examples. Normally I find it best to go file > new > MQX4.1 project and choose the example I want so I can select my cyclone debugger and have all the paths configured correctly. But you cant create 4.2 examples, the option is just not there in CW10.7.

I need to use the MQX Shell examples for RTCS. I tried file > new > MQX4.1 select the RTCS shell example, then changing the folder to MQX4.2 but it turns out the shell is completely different and it wont work. So I then resorted to "import project" and imported the MQX example project into my work space but the debugger is not there and its not enjoying me manually changing it.

Anyway, is there a reason MQX4.2 example applications cannot be created "the normal way"?

0 Kudos
Reply
1 Reply

1,006 Views
danielchen
NXP TechSupport
NXP TechSupport

Hi Carl Norman:

I think you need to update your codewarrior.  And update all options with MQX related.

Please refer to the following link for details, it is for 10.6, but  I think it is same for 10.7

https://community.nxp.com/message/576567 

 

Regards

Daniel

0 Kudos
Reply