Feature Request for Kinetis: DMA for UARTs

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Feature Request for Kinetis: DMA for UARTs

1,577 Views
Fabi
Contributor III

It would be great, if DMA will be supported for UARTs. The use-case is to send and receive about 100 Bytes every 5 msec with 460 KBaud. Using ittya: is my current solution, but it decelerates the system noticeable.

PLS, could freescale add it into the feature request list for MQX 3.9 or 4.0?

0 Kudos
Reply
2 Replies

1,249 Views
KJFPE
Contributor III

Try the USB virtual comm port which will be able to go at the speed you require

0 Kudos
Reply

1,249 Views
Fabi
Contributor III

@HJFPE Thanks for the hint. The use case is, however, inter processor communication inside an embedded device. SPI is not an option (because of reduced feature set of the other processor) as well as USB, too.

0 Kudos
Reply