Fatal error: P&E Connection layer supports only Cortex M3/M4 devices. Session aborted!

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Fatal error: P&E Connection layer supports only Cortex M3/M4 devices. Session aborted!

1,567 Views
davidcav
Contributor II

When I load the TWR-K60N512_Quick_Start_Demo project, I get the following error

 

Tue Mar 01 14:45:47 2011: Fatal error: P&E Connection layer supports only Cortex M3/M4 devices.   Session aborted!

 

- then when I try to make the project I get many errors ("cannot find file") and the project does not build.  The MQX librarires built fine.  I am using IAR Embedded workbench IDE 6.10.  It seems like the project is not pulling in the libraries correctly, but I do not also understand the original error message.

 

any help

0 Kudos
Reply
1 Reply

1,290 Views
KJFPE
Contributor III

Hi 

 

Right click on your project and select General option and select device Freescale K60Xxxx

 

Screen shot