FXOS8700CQ file pointer "MQX_FILE_PTR". unknown data type

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

FXOS8700CQ file pointer "MQX_FILE_PTR". unknown data type

3,908 Views
stevenbell11
Contributor I

FXOS8700CQ: Datasheet page 26 example code lists a file pointer "MQX_FILE_PTR". When I compile the code I get an error saying it is an unknown data type, do you know how to fix this?

0 Kudos
Reply
2 Replies

3,424 Views
Sudhar_27102001
Contributor I

can u give me the driver code for fxo8700cq. Facing sensor initialization failed error.in FRDM-K32L2B3 BOARD. pls help me on this.

0 Kudos
Reply

3,750 Views
danielchen
NXP TechSupport
NXP TechSupport

Hi  Steven

I would suggest you refer to the below document, it includes an example code written for Frdm-k64F board, using polled i2c MQX driver for communication  with FXOS8700CQ chip.

Accelerometer and magnetometer FXOS8700CQ example code for MQX4.1.1 

I hope it helps


Have a great day,
Daniel

-------------------------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button or helpful. Thank you!
---------------------------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply