Hi,
Im using MQX4.1 on FRDM-K64F board.
Now I create a project to setup a TelnetServer and use it to print some messages to the Client.
I have used func '_io_set_handle()' to change the handle of stdout/stdin, but it doesnt work well.
It means when i use printf(), the message doesnt print on the client immediately, the message was printed after I input something from the client.
if(TELNETSRV_telnetfd!=NULL) { _io_set_handle(IO_STDIN, TELNETSRV_telnetfd); _io_set_handle(IO_STDOUT, TELNETSRV_telnetfd); } printf("hwtimer1_callback...\n"); TELNETSRV_telnetfd is a global MQX_FILE_PTR value that I added in telnsrv.c
TELNETSRV_telnetfd held the value of telnetfd in TELNETSRV_child()
Here is the code...
Original Attachment has been moved to: testboard.zip
Hi Yang,
we need to investigate more about this issue and reproduce it. Could you submit a Service Request at www.freescale.com/support please?
Best regards,
Carlos Musich
Technical Support Engineer
Hi Carlos,
Yes I will do that.
Thanks & Regards,
Yang Dongxuan