FFS Mutex problem.

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

FFS Mutex problem.

868件の閲覧回数
danielchai
Senior Contributor I

Hi All,

Now I installed the FFS patch on MQX4.0.2 on TWRK60F120M.

And I installed the wear leveling without installing MFS on NAND FLASH.

When I try to use read/write NAND FLASH in a interrupt, it prints: "assertion failed: 0, file simple_mutex.cpp, line 141".

After digging into it, I found it can not lock the mutex because it can lock the mutex in a interrupt.

Do anyone have any ideas how can use read/write based on FFS in a interrupt?

Thank you.

-Daniel

0 件の賞賛
返信
0 返答(返信)