FFS MQX 4.0.2

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

FFS MQX 4.0.2

2,001 Views
okaner
Contributor III

After I pass to MQX 4.0.2, I have nandflash size problem. I get "Free disk space: 126212096 bytes" message instead of 252694528.

I installed mqx 4.0.2 and new ffs. I have done same steps but now I get smaller disk size. Do you have any idea.I use TWRK60f120m. I was successful on mqx 4.0.1.

previous discussion

Change size of FFS drive (MQX 4.0.1, TWR-K70)

nandflash_wl_ffs.h

#define NANDFLASH_1ST_DATA_DRIVE_SIZE_IN_BLOCK 1937

#define NANDFLASH_1ST_DATA_DRIVE_START_BLOCK 110

Formating...                                                             
Done. Volume name is                                                     

Free disk space: 126212096 bytes

Okan ERCAN

Tags (2)
0 Kudos
Reply
2 Replies

1,615 Views
danielchai
Senior Contributor I

Hi Okan ERCAN,

I am facing the same problem. Did you ever figure it out?

A question is where did you download the FFS_MQX 4.0.1, because I can only find the FFS patch for MQX4.0.2?

Thank you.

-Daniel

0 Kudos
Reply

1,615 Views
DavidS
NXP Employee
NXP Employee

Answered in following post:

Re: Re: Change size of FFS drive (MQX 4.0.1, TWR-K70)

Regards,

David

0 Kudos
Reply