EzPort programmer

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 
1,482件の閲覧回数
amleng
Contributor IV

Hi all,

I use EzPort programmer explained in AN4406. I could program small s19 files (less than 20K) but I have problem with larger files (100K). Is it fw limitation or something else?

Regards,

0 件の賞賛
返信
1 解決策
1,126件の閲覧回数
drummer
Contributor IV

I found that I had to decrease the reset pull up resistance to 4k7.

I am using the dediprog programmer in production.

I had so many problems when I first started.

I eventually figured out that 10K pull-ups are not quite strong enough.

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
1,127件の閲覧回数
drummer
Contributor IV

I found that I had to decrease the reset pull up resistance to 4k7.

I am using the dediprog programmer in production.

I had so many problems when I first started.

I eventually figured out that 10K pull-ups are not quite strong enough.

0 件の賞賛
返信