External MRAM

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

External MRAM

2,205 Views
admin
Specialist II

I'm developing on MQX an USB Host that read and save a configuration from an USB mass storage (USB device), an external MRAM is mandatory? I saw that MFS and USB Host use a lot of RAM ... an application of example inside MQX like \Freescale MQX 3.5\mfs\examples\mfs_usb can work correctly without external RAM?

Labels (1)
Tags (1)
0 Kudos
Reply
1 Reply

1,172 Views
cutworth
NXP Employee
NXP Employee

Of course you can implement a demo with only internal RAM, MCF52259 has 64KB on-chip RAM which should be enough for this purpose, MRAM is not mandatory.