Example for using the basic printer class?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Example for using the basic printer class?

1,423 Views
gorakk
Contributor IV

Is there a sample application for using the USB host printer class?

I have CodeWarrior 10.3 and MQX 4.0 installed.  There are examples for USB keyboard, mouse, etc but none for printer that I can see.

Thanks

Labels (1)
0 Kudos
Reply
1 Reply

1,110 Views
gorakk
Contributor IV

Just a quick update on this one - a Freescale rep suggested looking at the bare metal Freescale USB Stack for an example of printer support.  The USB Stack supports USB printers and does have an example.  I loaded the printer example into a tower system and (with a few code additions) it is able to print to a Godex DT2 printer.

I am now in the process of porting the printer example over to my MQX project.   Has anyone attempted this already?

I will update this thread again when I get further along.

For what it's worth - my MQX project is already working with USB keyboards and USB flash drives.

0 Kudos
Reply