Ethernet phy drivers

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Ethernet phy drivers

1,672件の閲覧回数
simonatoumberto
Contributor I

We are developing a  K60 board and we have to choose

a Ethernet phy Chip suitable.

The evaluation board uses KSZ8041NL (Micrel) that handles both mode MII RMII
but we wish to use one with only interface RMIII ex:  KSZ8081RNBIA

MQX drivers are compatible with this chip?

thanks
Umberto Simonato

0 件の賞賛
返信
1 返信

1,444件の閲覧回数
Luis_Garabo
NXP TechSupport
NXP TechSupport

Hi Umberto,

If the driver is close enough to what would be required for the 8081, you can modify the definitions in the phy_ksz8041.h header to match the 8081. It is just a matther of register address modification and so on.


Regards,
Garabo

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信