Error when dragging wsd file into workspace

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

Error when dragging wsd file into workspace

跳至解决方案
1,268 次查看
MWMinor
Contributor V

Hi

I am experiencing an issue with trying to drag the .wsd file created from the cloning wizard into my workspace.

I'm using CW V10.6.4 and MQX V4.1

The cloning wizard runs with no errors and generates the .xml and .reg files correctly.

I copy the .xml file into the ....\MCU\lib\wizard_data\mqx\4.1\arm directory and update the registry (I'm running 64-bit Windows 7 pro) but when I try to drag the .wsd file into the workspace, I just get an "error occ..." dialogue with a white cross in a red circle back ground and OK button to continue.

pastedImage_1.png

I have tried dragging some older (6 months plus) .wsd BSP files into the same workspace and they work fine.

Any ideas please...?

Thanks

Ken

1 解答
1,180 次查看
MWMinor
Contributor V

Problem solved.

There seems to be a maximum number of characters permitted in the new BSP name.

By keeping the number of characters to less than or equal to 11, the problem goes away

在原帖中查看解决方案

1 回复
1,181 次查看
MWMinor
Contributor V

Problem solved.

There seems to be a maximum number of characters permitted in the new BSP name.

By keeping the number of characters to less than or equal to 11, the problem goes away