Error when dragging wsd file into workspace

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Error when dragging wsd file into workspace

ソリューションへジャンプ
1,329件の閲覧回数
MWMinor
Contributor V

Hi

I am experiencing an issue with trying to drag the .wsd file created from the cloning wizard into my workspace.

I'm using CW V10.6.4 and MQX V4.1

The cloning wizard runs with no errors and generates the .xml and .reg files correctly.

I copy the .xml file into the ....\MCU\lib\wizard_data\mqx\4.1\arm directory and update the registry (I'm running 64-bit Windows 7 pro) but when I try to drag the .wsd file into the workspace, I just get an "error occ..." dialogue with a white cross in a red circle back ground and OK button to continue.

pastedImage_1.png

I have tried dragging some older (6 months plus) .wsd BSP files into the same workspace and they work fine.

Any ideas please...?

Thanks

Ken

1 解決策
1,241件の閲覧回数
MWMinor
Contributor V

Problem solved.

There seems to be a maximum number of characters permitted in the new BSP name.

By keeping the number of characters to less than or equal to 11, the problem goes away

元の投稿で解決策を見る

1 返信
1,242件の閲覧回数
MWMinor
Contributor V

Problem solved.

There seems to be a maximum number of characters permitted in the new BSP name.

By keeping the number of characters to less than or equal to 11, the problem goes away