Error when dragging wsd file into workspace

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Error when dragging wsd file into workspace

Jump to solution
1,266 Views
MWMinor
Contributor V

Hi

I am experiencing an issue with trying to drag the .wsd file created from the cloning wizard into my workspace.

I'm using CW V10.6.4 and MQX V4.1

The cloning wizard runs with no errors and generates the .xml and .reg files correctly.

I copy the .xml file into the ....\MCU\lib\wizard_data\mqx\4.1\arm directory and update the registry (I'm running 64-bit Windows 7 pro) but when I try to drag the .wsd file into the workspace, I just get an "error occ..." dialogue with a white cross in a red circle back ground and OK button to continue.

pastedImage_1.png

I have tried dragging some older (6 months plus) .wsd BSP files into the same workspace and they work fine.

Any ideas please...?

Thanks

Ken

1 Solution
1,178 Views
MWMinor
Contributor V

Problem solved.

There seems to be a maximum number of characters permitted in the new BSP name.

By keeping the number of characters to less than or equal to 11, the problem goes away

View solution in original post

1 Reply
1,179 Views
MWMinor
Contributor V

Problem solved.

There seems to be a maximum number of characters permitted in the new BSP name.

By keeping the number of characters to less than or equal to 11, the problem goes away