Error opening filesystem:

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Error opening filesystem:

2,232件の閲覧回数
haoyuancai
Contributor II

Dear all:

I have a problem when I use SD card. I attached my code before. I found the return value is error when I use fopen = ("a:",NULL); the return value is 0x000000.

I dont know why?

void main(void)

{

     (void)          temp; /* suppress 'unused variable' warning */

      boolean            inserted = TRUE, readonly = FALSE, last = FALSE;

    _mqx_int        error_code;

    _mqx_uint       param;

    MQX_FILE_PTR    com_handle, sdcard_handle, filesystem_handle, partition_handle;

    char            filesystem_name[] = "MFS:";

    char            partman_name[] = "pm:";

    char            partition_name[] = "pm:1";

com_handle = fopen(BSP_SDCARD_ESDHC_CHANNEL, (void *)(SPI_FLAG_FULL_DUPLEX));

error_code = _io_sdcard_install("sdcard:", (void *)&_bsp_sdcard0_init, com_handle);

sdcard_handle = fopen("sdcard:", 0);

       /* Install MFS over SD card driver */

error_code = _io_mfs_install(sdcard_handle, filesystem_name,0);

(The return value is all correct above)

filesystem_handle = fopen(filesystem_name, NULL);  (filesystem_handle  is equal to 0x00000000) and mention "Error open filesystemname" But I think I can open the sdcard device. Therefore, there is not problem in hardware? right ?

error_code = ferror(filesystem_handle);

}

Any one can help me .thankyou

ラベル(1)
0 件の賞賛
返信
3 返答(返信)

2,038件の閲覧回数
haoyuancai
Contributor II

I use the demo board that design by myself. I realize this function before. Due to my issue, I lost my program. so I did again. the version of MQX is 4.0.         I try the sdcard example , but I found the program would be dead when it execute (filesystem_handle = fopen(filesystem_name, NULL); ). I use debuger to debug step by step.

In addition ,I have try 2G sd card and 16G sd card.

                                                                                                                                           Thx sol.

0 件の賞賛
返信

2,038件の閲覧回数
soledad
NXP Employee
NXP Employee

Hi,

Are you using a Freescale board?

Which MQX version are you using?

Could you please try using the sdcard example in order to discard a software or hardware issue? This example is located at the path:  C:\Freescale\Freescale_MQX_4_2\mfs\examples\sdcard

Could you please try using different sd card brands and capacities?

If you are using a Freescale board, could you please double check the jumper settings?


Have a great day,
Sol

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信

2,038件の閲覧回数
haoyuancai
Contributor II

Besides ,I also found I can read and write the block in SD card . But I can not install a mfs filesystem inside.

0 件の賞賛
返信