Hi,
I am using M52259 CW7.2 and MQX3.8. right now i want to use Mutex in my applcation. I would like to know if i need to enable anything before I start using mutexes.
According to MQX user manual section 3.6.6 , the Mutex component is not compiled in the MQX kernel by default. so I should enable it in (config.h ?) and re-build the whole MQX before i use it in my application . But i have not done anything in config.h, and the the mutex works well so far.
could anybody advise?
Thank you,
Weining
已解决! 转到解答。
C:\Program Files\Freescale\Freescale MQX 3.X\mqx\source\include
C:\Program Files\Freescale\Freescale MQX 3.X\mqx\source\mutex
in the C:\Program Files\Freescale\Freescale MQX 3.X\mqx\source\include have a look in mqx_cnfg.h