Delay in microsecond

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 
8,373件の閲覧回数
amleng
Contributor IV

Hello,

How can I generate delay in microsecond scale in MQX? _time_delay() works in ms only. I need it for 1-wire memory protocol.

Regards,

1 解決策
2,591件の閲覧回数
Martin_
NXP Employee
NXP Employee

Typically, default BSP resolution for an MQX tick is 5 ms. So, _time_delay_ticks(1) would put the task back to ready queue 5 milliseconds after the call to it. To get a finer resolution, you can use _time_get_microseconds or _time_get_nanoseconds functions, or even _time_get_hwticks.

If your time delay range is in microseconds, a wait function like the example below works. On TWR-MCF52259 this code gives me about 6 microseconds delay. This kind of delay function should be considered as a minimum delay, due to possible MQX preemptions by higher priority task(s), MQX interrupt(s) and so forth.

   #define MIN_DELAY_HWTICKS    (10)

   /* write logical 1 to the pin - initial state */

   lwgpio_set_value(&led1, LWGPIO_VALUE_HIGH); /* set pin to 1 */

  

   /* write logical 0 to the pin - falling edge - delay starts */

   lwgpio_set_value(&led1, LWGPIO_VALUE_LOW); /* set pin to 0 */

  

   /* do nothing for minimum 10 hwticks plus some software overhead */

   old_hwticks = _time_get_hwticks();

   diff_hwticks = 0;

   while(MIN_DELAY_HWTICKS > diff_hwticks)

   {

     hwticks = _time_get_hwticks();

     /* get the time elapsed from old_hwticks.

      * we need to consider a possible occurrence of a tick

      * between the two _time_get_hwticks() calls.

      * if a tick occurs between the two, it is possible that old_hwticks

      * is a greater value than the actual hwticks

      * (because a tick resets hwticks to 0)

      */

     diff_hwticks = hwticks>old_hwticks?(hwticks-old_hwticks):((int_32)_time_get_hw_ticks_per_tick()-old_hwticks+hwticks);

   }

  

   /* write logical 1 to the pin */

   lwgpio_set_value(&led1, LWGPIO_VALUE_HIGH); /* set pin to 1 */

元の投稿で解決策を見る

1 返信
2,592件の閲覧回数
Martin_
NXP Employee
NXP Employee

Typically, default BSP resolution for an MQX tick is 5 ms. So, _time_delay_ticks(1) would put the task back to ready queue 5 milliseconds after the call to it. To get a finer resolution, you can use _time_get_microseconds or _time_get_nanoseconds functions, or even _time_get_hwticks.

If your time delay range is in microseconds, a wait function like the example below works. On TWR-MCF52259 this code gives me about 6 microseconds delay. This kind of delay function should be considered as a minimum delay, due to possible MQX preemptions by higher priority task(s), MQX interrupt(s) and so forth.

   #define MIN_DELAY_HWTICKS    (10)

   /* write logical 1 to the pin - initial state */

   lwgpio_set_value(&led1, LWGPIO_VALUE_HIGH); /* set pin to 1 */

  

   /* write logical 0 to the pin - falling edge - delay starts */

   lwgpio_set_value(&led1, LWGPIO_VALUE_LOW); /* set pin to 0 */

  

   /* do nothing for minimum 10 hwticks plus some software overhead */

   old_hwticks = _time_get_hwticks();

   diff_hwticks = 0;

   while(MIN_DELAY_HWTICKS > diff_hwticks)

   {

     hwticks = _time_get_hwticks();

     /* get the time elapsed from old_hwticks.

      * we need to consider a possible occurrence of a tick

      * between the two _time_get_hwticks() calls.

      * if a tick occurs between the two, it is possible that old_hwticks

      * is a greater value than the actual hwticks

      * (because a tick resets hwticks to 0)

      */

     diff_hwticks = hwticks>old_hwticks?(hwticks-old_hwticks):((int_32)_time_get_hw_ticks_per_tick()-old_hwticks+hwticks);

   }

  

   /* write logical 1 to the pin */

   lwgpio_set_value(&led1, LWGPIO_VALUE_HIGH); /* set pin to 1 */