Debugging from CW 10.6 in virtual machine with windows 7

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Debugging from CW 10.6 in virtual machine with windows 7

2,190 Views
gbg77
Contributor I

Hello everyone I could compile my first mqx example, but When I try to run the debugger it just hangs on the initialization step. I am using  TWR-K60D100M code warrior 10.6.

in  virtual machine with windows 7.

This appear "Error creating session: The CodeWarrior Debugger Engine exited prematurely. Your installation may be corrupt."

Does someone can help me? Any suggestions?

Thanks

Tags (1)
0 Kudos
Reply
1 Reply

1,976 Views
Carlos_Mendoza
NXP Employee
NXP Employee

Hi Gabriela,

Which native OS are you using? Maybe Kinetis Design Studio is a better option for you, it is supported in Windows® 7/8, Linux® (Ubuntu 14.04 and RedHat/Centos 7) and Mac OS X ("Yosemite"), this way you don't have to use a virtual machine and avoid having problems with the installation and drivers.

Here is the link the KDS website:

Kinetis Design Studio Integrated Development |Freescale

Hope it helps!

Best Regards,

Carlos Mendoza

Technical Support Engineer

0 Kudos
Reply