Data flash driver

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Data flash driver

Jump to solution
4,416 Views
Teckna
Contributor V

I know that MQX 3.8 is going to be released in few days. Is there any rumors about the MFS data flash driver?

I'm using AT45DB161D data flash on which I want to put a file system and this driver would be much useful.

 

Many thanks

Teckna

Labels (1)
Tags (1)
0 Kudos
Reply
1 Solution
3,890 Views
c0170
Senior Contributor III

Hi Teckna,

 

Negative answer. There is no data flash driver in MQX 3.8.

 

Regards,

MartinK

View solution in original post

0 Kudos
Reply
8 Replies
3,891 Views
c0170
Senior Contributor III

Hi Teckna,

 

Negative answer. There is no data flash driver in MQX 3.8.

 

Regards,

MartinK

0 Kudos
Reply
3,890 Views
Teckna
Contributor V

Hi Martin,

What about data flash driver in the upcoming MQX 4.0?

Many thanks

Teckna

0 Kudos
Reply
3,890 Views
JuroV
NXP Employee
NXP Employee

There is nandflash driver with wear leveling functionality in MQX 4.0 AFAIK.

3,890 Views
BryGuyH
Contributor IV

I've been looking for it in the MQX 4.0 release and can't seem to find it. I've gone through all the K60/K70 projects and haven't seen anything jump out at me regarding a wear leveling module present. Can you point me in the right direction?

0 Kudos
Reply
3,890 Views
JuroV
NXP Employee
NXP Employee

Hi Bryant,

excuse me for misinformation. I was informed that the package will be released soon separately for MQX 4.0

0 Kudos
Reply
3,890 Views
markusp
Contributor I

This separate package - are you referring to the Embedded Access's SFFS add-on, or will there be another, free package added to the MQX 4.0? When it will be released?

Br,

Markus

0 Kudos
Reply
3,890 Views
JuroV
NXP Employee
NXP Employee

I asked for an information why it was still not released. The reply was that you should ask Freescale's customer support to get status of this package.

It is NOT the one from Embedded Access.

0 Kudos
Reply
3,890 Views
Teckna
Contributor V

Is there any plan to develope such driver in the future release of MQX?

 

Many thanks

Teckna

0 Kudos
Reply