Good afternoon:
I’m triying to use the D4D library on a custom pcb using the MK53DN512CMD10 microcontroller but I have some troubles. At the beginning I used the TWRK53N512 and I didn’t have troubles starting the LCD (NHD-1.8-128160EF). The custom pcb is connected as shown on the table.
TOUCH-SCREEN | MICROCONTROLLER PIN NAME |
CS | PTC9 |
RST | PTC10 |
D/C | PTC11 |
WR | PTC12 |
RD | PTC13 |
DB0 | PTC0 |
DB1 | PTC1 |
DB2 | PTC2 |
DB3 | PTC3 |
DB4 | PTC4 |
DB5 | PTC5 |
DB6 | PTC6 |
DB7 | PTC7 |
Y+ | ADC1_DM1/ OP1_DM0 |
Y- | PGA1_DP/ ADC1_DP0/ ADC0_DP3 |
X+ | PGA1_DM/ ADC1_DM0/ ADC0_DM3 |
X- | ADC1_SE16/ OP1_OUT/ CMP2_IN2/ ADC0_SE22/ OP0_DP2/ OP1_DP2 |
LED-A | DAC0_OUT/ CMP1_IN3/ ADC0_SE23/ OP0_DP4/ OP1_DP4 |
I already changed this pin configurations on the d4dlcdhw_gpio8080_8b_cfg.h file as follow:
* Signals definition
*******************************************/
#define D4DLCD_CS 9 // CS
#define D4DLCD_DC 11 // DC
// I/O port CONFIG for parallel transfer
#define D4DLCD_WR 12 // WRITECLOCK
#define D4DLCD_RD 13 // READCLOCK
/*********** Power macros - for modification uncoment and modify ***********/
// Define void macros, because
#define D4DLCD_INIT_CS SIM_SCGC5 |= SIM_SCGC5_PORTC_MASK;\
CONFIG_PIN_FUNCTION(C,9,1);\
OUTPUT(C,9)
#define D4DLCD_ASSERT_CS WRITE_PIN(C,9,0);
#define D4DLCD_DEASSERT_CS WRITE_PIN(C,9,1);
// Define void macros, because
#define D4DLCD_INIT_DC SIM_SCGC5 |= SIM_SCGC5_PORTC_MASK;\
CONFIG_PIN_FUNCTION(C,11,1);\
OUTPUT(C,11)
#define D4DLCD_ASSERT_DC WRITE_PIN(C,11,1);
#define D4DLCD_DEASSERT_DC WRITE_PIN(C,11,0);
// Define void macros, because
#define D4DLCD_INIT_RD SIM_SCGC5 |= SIM_SCGC5_PORTC_MASK;\
CONFIG_PIN_FUNCTION(C,13,1);\
OUTPUT(C,13)
#define D4DLCD_ASSERT_RD WRITE_PIN(C,13,0);
#define D4DLCD_DEASSERT_RD WRITE_PIN(C,13,1);
// Define void macros, because
#define D4DLCD_INIT_WR SIM_SCGC5 |= SIM_SCGC5_PORTC_MASK;\
CONFIG_PIN_FUNCTION(C,12,1);\
OUTPUT(C,12)
#define D4DLCD_ASSERT_WR WRITE_PIN(C,12,0);
#define D4DLCD_DEASSERT_WR WRITE_PIN(C,12,1);
// Define void macros, because
#define D4DLCD_INIT_DATA SIM_SCGC5 |= SIM_SCGC5_PORTC_MASK;\
CONFIG_PIN_FUNCTION(C,0,1);\
OUTPUT(C,0);\
CONFIG_PIN_FUNCTION(C,1,1);\
OUTPUT(C,1);\
CONFIG_PIN_FUNCTION(C,2,1);\
OUTPUT(C,2);\
CONFIG_PIN_FUNCTION(C,3,1);\
OUTPUT(C,3);\
CONFIG_PIN_FUNCTION(C,4,1);\
OUTPUT(C,4);\
CONFIG_PIN_FUNCTION(C,5,1);\
OUTPUT(C,5);\
CONFIG_PIN_FUNCTION(C,6,1);\
OUTPUT(C,6);\
CONFIG_PIN_FUNCTION(C,7,1);\
OUTPUT(C,7);\
OUTPUT_ALL(C)
#endif /* __D4DLCDHW_GPIO8080_8B_CFG_H */
And with this configuration doesn’t appear anything on the LCD. I verified every signal, and I noticed that on pin 6(D/C-Data/Command selection) the signal is like this

And the signal of the tower, where the code works, is like this

I think the signal in this pin is the problem, cause the other signals are the same in both boards.
Did I miss change something in the code? What could be a solution for this trouble?
I will apreciate a lot your help !!!!!
Best Regards