Creating new MQX 3.7 Project with PE?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

Creating new MQX 3.7 Project with PE?

跳至解决方案
1,728 次查看
lowks
Contributor III

Hi, is it possible to enable PE when using creating a new MQX 3.7 project? I realised that I cannot enable PE when I tried to create a K40 or K60 MQX project.

0 项奖励
回复
1 解答
1,497 次查看
LuisCasado
NXP Employee
NXP Employee

Hello,

 

There is not differences to create a new MQX project with PE or non PE. You can use the same wizard option, the BSP used in your project will be the last built. If the last BSP built is the PE enabled, you new project is PE enabled. The BSP libs included in your new projects are in the same place for BSP with or without BSP enabled.

 

Best Regards,

在原帖中查看解决方案

0 项奖励
回复
4 回复数
1,497 次查看
DavidS
NXP Employee
NXP Employee

Hi Iowks,

Please review C:\Program Files\Freescale\Freescale MQX 3.7\doc\FSL_MQX_3_7_in_CW_10_1.pdf starting on page 89.

It walks you through using PE with K60 or K40.

Hope this helps.

Regards,

David

0 项奖励
回复
1,497 次查看
lowks
Contributor III

i saw this portion in the document and have tried it before. I am just wondering since there is such a function called "Create new MQX 3.7 Project" and allows user to choose the BSP, why using this option does not allow PE to be activated? Then this option is not that useful to the user.

0 项奖励
回复
1,498 次查看
LuisCasado
NXP Employee
NXP Employee

Hello,

 

There is not differences to create a new MQX project with PE or non PE. You can use the same wizard option, the BSP used in your project will be the last built. If the last BSP built is the PE enabled, you new project is PE enabled. The BSP libs included in your new projects are in the same place for BSP with or without BSP enabled.

 

Best Regards,

0 项奖励
回复
1,497 次查看
LuisCasado
NXP Employee
NXP Employee

Hello,

 

Sorry, I meant : "....with or without PE enabled"

 

Best Regards,

0 项奖励
回复