Console using debugging port

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Console using debugging port

1,867件の閲覧回数
Ardoster
Contributor III

Hi

 

I'm using a M5229DEMOKit with a Developpment Studio CodeWarrior.

 

I would like to redirect the printf output to the usb port used for debugger (OSBDM), but I have no idea to do this. Is this possible? I think is possible, because when I create a Coldfire proyect without using MQX, is disposable a target called CONSOLE_INTERNAL_RAM, which redirect my printf outuput to an internal console in my coldfire. But this target is not disposable when I create a MQX project.

 

Do you have any suggestion?

 

Thanks you in advance.

0 件の賞賛
返信
1 返信

1,268件の閲覧回数
Ardoster
Contributor III

Hi

 

I've found this another thread (http://forums.freescale.com/freescale/board/message?board.id=CFCOMM&message.id=2864&query.id=32052#M...) where its explained how redirect the printf output via OSBDM port, using a little console opened in Codewarrior. I've tested it with a basic coldfirer project (no MQX) and it runs correctly.

 

But, How I could adapt it to an MQX projec, where I don't have for example an exceptions.c file, like in a basic coldfire project?

 

Thanks you in advance

Message Edited by Ardoster on 2009-09-08 09:46 AM
0 件の賞賛
返信