Connection TCP timeout

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

Connection TCP timeout

跳至解决方案
16,118 次查看
diegoderganz
Contributor II

Enviroment: M52259 demo board with MQX3.6 on CW 7.2

I have connect the M52259 board to my PC and a UMTS router thru the ethernet port.

I have to make a TCP connection to a server thru the UMTS router.

I can make the connection to my PC and from my PC to the server (thru the UMTS router using telnet), but I can't connect the board directly to the remote server (connection timeout).

Can be a problem with packet latency or else to estabilish the connection?

Thanks,

Diego Derganz

Lists attatched below:

void TCPClient(void)

{

    sockaddr_in    addr;

    _ip_address    ipaddr;

    uint_32        error;

    uint_32        option;

   

    char        buffer[TCPCLIENT_RECV_BUF_SIZE];

//    sockaddr    server_socket_addr;

   

    uint_32     socket_handle;

   

//    _ip_digital digit;

    uint_32     opt_val;

    uint_32     opt_len;

    ipaddr = Server_addr;

    printf("\n[TCPClient]: Launching TCPClient...");

    opt_val = 3 * 60 * 1000;

    opt_len = sizeof(uint_32);

    // set remote host(TCPServer) socket address

//    server_socket_addr.sin_family      = AF_INET;

//    server_socket_addr.sin_port        = port;

//    server_socket_addr.sin_addr.s_addr = ip;

    // loop to establish connection

    do {

        // Create a stream socket for TCPClient.

        socket_handle = socket(AF_INET, SOCK_STREAM, 0);

        if (socket_handle == RTCS_SOCKET_ERROR) {

            printf("\n[TCPClient]: Failed to create socket.");

            _task_block();

        }

        option = 10000;    // 10 sec  

        error = setsockopt(socket_handle, SOL_TCP, OPT_RETRANSMISSION_TIMEOUT, &option, sizeof(option));

//        Reduce buffer size of socket to save memory

        option = 512;  

        error = setsockopt(socket_handle, SOL_TCP, OPT_TBSIZE, &option, sizeof(option));

        option = 512;  

        error = setsockopt(socket_handle, SOL_TCP, OPT_RBSIZE, &option, sizeof(option));

        option = 1000;

        error = setsockopt(socket_handle, SOL_TCP, OPT_TIMEWAIT_TIMEOUT, &option, sizeof(option));

        // set 3mins for connection Timeout

        option = 3 * 60 * 1000;

        error = setsockopt(socket_handle, SOL_TCP, OPT_CONNECT_TIMEOUT, &option, sizeof(option));

        if (error != RTCS_OK) {

            printf("\n[TCPClient]: Failed to setsockopt for OPT_CONNECT_TIMEOUT, CODE = 0x%x.", error);

            _task_block();

        }

        // try to connect TCPServer

        addr.sin_port        = 2600;

        addr.sin_addr.s_addr = ipaddr;

        error = connect(socket_handle, &addr, sizeof(addr));

        if (error != RTCS_OK) {

            if (error == RTCSERR_TCP_TIMED_OUT) {

                printf("\n[TCPClient]: Connection timeout.");

            } else if (error == RTCSERR_TCP_CONN_RESET) {

                printf("\n[TCPClient]: Connection reset by peer."); // When connect to PC but TCPServer shuntdown, will alert this error

            }

            shutdown(socket_handle, FLAG_ABORT_CONNECTION);

            printf("\n[TCPClient]: Retry to connect TCPServer 5 seconds later...");

            _time_delay(5 * 1000);

        }

    } while (error != RTCS_OK);

//    // display connection message

//    ip_to_digital(ip, &digit);

//    printf("\n[TCPClient]: Connected to TCPServer, IP = %d.%d.%d.%d, Port = %d.",

//           digit.high, digit.middlehigh, digit.middlelow, digit.low, port);

    printf("\n[TCPClient]: Connected.");

     // clean buffer to ensure '\0' filled for recv

    memset(buffer, 0, sizeof(buffer));

   

    while (TRUE) {

        // Send msg to TCPServer

        if (send(socket_handle,

                 "I'm TCPClient. Please reply to me.", strlen("I'm TCPClient. Please reply to me") + 1,

                 0) == RTCS_ERROR) {

            printf("\n[TCPClient]: Failed to send, CODE = 0x%x.", RTCS_geterror(socket_handle));

            _task_block();

        }

        // wait to receive msg from TCPServer

        if (recv(socket_handle, buffer, sizeof(buffer), 0) == RTCS_ERROR) {

            error = RTCS_geterror(socket_handle);

            // Close TCPClient if TCPServer close first.

            if (error == RTCSERR_TCP_CONN_CLOSING) {

                shutdown(socket_handle, FLAG_ABORT_CONNECTION);

                printf("\n[TCPClient]: Closed.");

                break;

            // Close TCPClient if TCPServer abort.

            } else if (error == RTCSERR_TCP_CONN_RESET) {

                shutdown(socket_handle, FLAG_ABORT_CONNECTION);

                printf("\n[TCPClient]: Connection reset by peer.");

                printf("\n[TCPClient]: Closed.");

                break;

            } else {

                printf("\n[TCPClient]: Failed to recv, CODE = 0x%x.", error);

                _task_block();

            }

        } else {

            printf("\n[TCPClient]: Received \"%s\".", buffer);

           

            // clean buffer to ensure '\0' filled for next recv.

            memset(buffer, 0, sizeof(buffer));

        }

    }

}

标签 (1)
标记 (2)
0 项奖励
回复
1 解答
11,667 次查看
diegoderganz
Contributor II

Now I have resolve the TCP/IP connection thru my router UMTS.

1) I have put a windows size = TCP_DEFAULT_RBSIZE in SYN packet.

2) Because I don't have found how to remove the trailing byte of the Ethernet frame I have put some option byte in the TCP frame to avoid this problem.

I think that it's a UMTS router problem, but can you put some define to patch (windows size in SYN packet and remove trailing byte in Ethernet frame) in the next version? So if another have the same problem can only modify the define.

Someone know how to remove the trailing bytes in the Ethernet frame?

Best regards,

Diego Derganz


在原帖中查看解决方案

0 项奖励
回复
8 回复数
11,667 次查看
diegoderganz
Contributor II

Now I have resolve the TCP/IP connection thru my router UMTS.

1) I have put a windows size = TCP_DEFAULT_RBSIZE in SYN packet.

2) Because I don't have found how to remove the trailing byte of the Ethernet frame I have put some option byte in the TCP frame to avoid this problem.

I think that it's a UMTS router problem, but can you put some define to patch (windows size in SYN packet and remove trailing byte in Ethernet frame) in the next version? So if another have the same problem can only modify the define.

Someone know how to remove the trailing bytes in the Ethernet frame?

Best regards,

Diego Derganz


0 项奖励
回复
11,667 次查看
michris
Contributor III

Hi,

Possible to share your code change? (line, file?)

Thx

Christophe

0 项奖励
回复
11,667 次查看
Martin_
NXP Employee
NXP Employee

I'm not sure if this is similar fix, but here is source code change for MQX 4.0.2 to put window with SYN packet.

https://community.freescale.com/message/356963#356963

0 项奖励
回复
11,667 次查看
diegoderganz
Contributor II

Using wireshark I have see that my router reject the SYN packet of TCP connection with windows size = 0 and I have put a patch on that.

Now I can make the TCP connection from device to the server (thru the router UMTS) only using my PC in the middle like a gateway.

The only thing that my PC do is to remove the trailing bytes added in the ethernet protocol.

Can someone tell me where I have to modify to remove the trailing bytes?

Best regards,

Diego Derganz

0 项奖励
回复
11,667 次查看
diegoderganz
Contributor II

Now I have try M52259EVB board with CW 10.4 and MQX 4.0.1

I have try web_hvac demo with webserver disabled and shell enabled.

I have enabled the telnet client, present in MQX, with a little modification to modify the default port.

Log:

Shell (build: Jun 26 2013)

Copyright (c) 2013 Freescale Semiconductor;

shell>

shell> ipconfig

Eth#: 0

Link: on

MAC : 00:00:5e:a8:01:02

IP4 : 192.168.1.2 type: MANUAL

MASK: 255.255.255.0

GATE: 192.168.1.1

DNS1: 8.8.8.8

Link status task stopped

shell>

shell> telnet 192.168.1.3 2600

Connecting to   [192.168.1.3] port 2600:

Connection closed

shell> ping *server*

Pinging 147.xx.xx.xx:

Press [q] to cancel.

Reply from [147.xx.xx.xx]: time=205ms

Reply from [147.xx.xx.xx]: time=195ms

Reply from [147.xx.xx.xx]: time=185ms

Request timed out

shell> telnet *server* 2600

Connecting to *server* [147.xx.xx.xx] port 2600:

Connection failed, error 0x1649

Connection closed

shell>

shell> ping 192.168.1.1

Pinging 192.168.1.1:

Press [q] to cancel.

Request timed out

Reply from [192.168.1.1]: time=10ms

Request timed out

Reply from [192.168.1.1]: time=10ms

shell>


It's normal that I have some request timed out in ICMP request?


How can I log all the traffic on the ethernet on the serial console?


Thanks,

Diego Derganz

0 项奖励
回复
11,667 次查看
Luis_Garabo
NXP TechSupport
NXP TechSupport

Hi Diego,

The first thing you need to confirm is that your PC or other device can see the board. That way you will ensure that the problem is not in the communication but at the application level. To probe this you can use a PING command from windows to the IP address of your board. If there is a free path between the board and your PC then you will get the PING answered. Next you will need to verify that the packages from your board are reaching your PC. You can use a ethernet sniffer for this (like wireshark). Next I would remove all the socket iptions and leave the default values until you can probe that there is a communication and that you can perform connections to the server.

My two cents...

Best Regards,

Garabo

0 项奖励
回复
11,667 次查看
diegoderganz
Contributor II

Hi Garabo,

the device normally is directly connected with the UMTS router to have access to the internet.

The device has a web server and has to connect sometime with an external server.

Because it can't work I have put another router in the middle to connect device (192.168.1.2), UMTS router (192.168.1.1) and my PC (192.168.1.3).

I can:

- see my device [web server] thru the internet (UMTS router redirect the connection to the device)

- see my device [web server] thru the local LAN (my PC)

- create TCP connection to internet server from my PC (test with telnet)

- create TCP connection to my PC from the device (local LAN)

I can't create the TCP connection from the device to the internet server thru the UMTS router.

Maybe there is some problem during the TCP handshake thru the UMTS router?

The gateway is well configured and I can resolve the DNS queries and receive date and time from SNTP service.

So the only difference from local LAN and internet server is that I have specify an IP outside the netmask, it's correct? I have to modify something else?

Any suggestions for the application layer?

Best regards,

Diego Derganz

0 项奖励
回复
11,667 次查看
diegoderganz
Contributor II

Any suggestions on how to debug the TCP connection to understand why it does not work and I get connection timeout?

0 项奖励
回复