Configure IPV6 route

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Configure IPV6 route

2,018件の閲覧回数
Coacci
Contributor II

Hello!
We are currently using a Wi-SUN Network, where the end-devices have IPV6 address in 2017::/64 range and they are accessible through a gateway on the network 2001 (2001::2). The Ethernet Interface of our communication board is connected directly to this gateway by a ethernet cable and was configured with the address 2001::1.

The initial idea was to send UDP datagrams from the board to one of the end-devices through the gateway, but it did not work (unfortunately we can't get the traffic in this scenario).

We did some tests using a directly communication between the board and a computer with Linux Ubuntu. We've sent the udp datagrams using IPV6 Link-Local Addresses (FE80::/64) and it worked pretty fine, we were able to get the traffic between theses two devices. But the problem is when we try to use another IPV6 address than fe80::/64, it just doesn't work.

With this, we have a scenario where link-local addresses work well in point-to-point communication, but any attempt to use global addresses fails, whether via Wi-SUN gateway or direct connection.

Is there any way to configure a route on RTCS IPV6? If it's not, how can we proceed?

タグ(4)
0 件の賞賛
返信
3 返答(返信)

1,985件の閲覧回数
danielchen
NXP TechSupport
NXP TechSupport

Hi @Coacci :

 

Now RTCS IPv6 is wrapped in MQX v5, under commercial license.  Please refer to below link for more details.

MQX™ v5 Software Solutions | NXP Semiconductors

If you need further information please contact MQX team at [email protected]

 

Regards

Daniel

0 件の賞賛
返信

1,980件の閲覧回数
Coacci
Contributor II

Hello! I forgot to mention that we are using MQX V4.2 + RTCS IPV6 addon that we've previously purchased with NXP.
Using v5 is not an option for us now, could you help us in this case?

0 件の賞賛
返信

1,964件の閲覧回数
danielchen
NXP TechSupport
NXP TechSupport

Please contact [email protected]  for IPv6 relevant questions

 

Regards

Daniel

0 件の賞賛
返信