Composite device with mqx usbd stack

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Composite device with mqx usbd stack

ソリューションへジャンプ
1,663件の閲覧回数
handychandra
Contributor III

Hi, i want to ask if it is possible to use mqx usbd stack to create usb device with two functions, say cdc and msd ? So computers will detect it as two device, cdc and msd.

ラベル(1)
タグ(3)
1 解決策
1,429件の閲覧回数
soledad
NXP Employee
NXP Employee

Hi Handy,

The theory says it is possible to use mqx usb stack to create usb device with cdc and msd, unfortunately we do not have an example to share with you based on MQX.

However, you can find MSD+CDC and HID+Audio+Video composite device examples that you could use as reference on bare-metal Freescale USB Stack v4.1, which can be found on www.freescale.com/medicalusb

Have a nice day!!!

Regards

Soledad

元の投稿で解決策を見る

1 返信
1,430件の閲覧回数
soledad
NXP Employee
NXP Employee

Hi Handy,

The theory says it is possible to use mqx usb stack to create usb device with cdc and msd, unfortunately we do not have an example to share with you based on MQX.

However, you can find MSD+CDC and HID+Audio+Video composite device examples that you could use as reference on bare-metal Freescale USB Stack v4.1, which can be found on www.freescale.com/medicalusb

Have a nice day!!!

Regards

Soledad