Codewarrior 10.5 and MQX Full Project

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Codewarrior 10.5 and MQX Full Project

1,234 Views
xianpingjiang
Contributor I

Hello. I have installed MQX 4.1, and I am using CW 10.5. I can only create an MQX Lite Project. Back when I had MQX 4.0 installed, I was able to either create a Lite or Full Project. How can I create an MQX Full project with MQX 4.1?

Thanks

0 Kudos
Reply
1 Reply

1,096 Views
danielchen
NXP TechSupport
NXP TechSupport

Hi Xianping

Please check the following link for your issue.

https://community.freescale.com/message/385205#385205


Have a great day,
Daniel

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply