CodeWarrior Not Found Even If it is Installed

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

CodeWarrior Not Found Even If it is Installed

ソリューションへジャンプ
2,250件の閲覧回数
RohanShah
Contributor I

Hi, 

I have Installed CodeWarrior for MCU v10.1 successfully & then I started installing MQX 3.6.2, its installer did searched for CodeWarrior as usual, but it failed to find it. (Please ref. screenshot attached).

Can anyone guide how I can link MQX with CodeWarrior workbench?

 

Thanks in advance.

0 件の賞賛
返信
1 解決策
1,709件の閲覧回数
petr_uhlir
NXP Employee
NXP Employee

Hi,

its because MQX 3.6.2 does not support TAD plugin for CodeWarrior for MCU v10.1 yet. It will be enabled  in next MQX release.

元の投稿で解決策を見る

0 件の賞賛
返信
2 返答(返信)
1,710件の閲覧回数
petr_uhlir
NXP Employee
NXP Employee

Hi,

its because MQX 3.6.2 does not support TAD plugin for CodeWarrior for MCU v10.1 yet. It will be enabled  in next MQX release.

0 件の賞賛
返信
1,708件の閲覧回数
TomR
Contributor I

I am having the same problem.

 

The only version of CodeWarrior 10 to download is version 10.1. Does this mean I can't do MQX development with CW10.1 and MQX 3.6.2?

0 件の賞賛
返信