I have written pc-relative routines in assembler. I want to relocate them to different memory devices on the tower board. I have selected both SDRAM and internal SRAM. In both cases, the relocation works after the 2nd attempt to use the memory after a hard reboot (disconnect power). If I do a soft reboot, then the routines are fine the first time. I have mqx running and implemented some primitive tz-monitor handling (the same issue happens with/without tz). I can see the code gets a DFSR of '0x00001c06'; the IFSR is 0x5 maybe these are irrelevant. I have examined the memory before/after the code update and the d-cache seems to say the code has been updated. I am using the following mqx code to try and synchronize the caches,
memcpy(p, (void*)target, size);
asm("dsb"); asm("isb");
_DCACHE_FLUSH();
asm("dsb"); asm("isb");
_ICACHE_INVALIDATE();
asm("dsb"); asm("isb");
_DCACHE_INVALIDATE();
asm("dsb"); asm("isb");
if(memcmp(p, (void*)target, size))
printf("Memory mismatch\n");
else
printf("Memory OK!\n");
/* Clear data/instruction fault registers. */
asm(" mcr p15, 0, %0, c6, c0, 0\n" :: "r"(0xaa55aa55UL));
asm(" mcr p15, 0, %0, c5, c0, 0\n" :: "r"(0xaa55aa55UL));
asm(" mcr p15, 0, %0, c6, c0, 2\n" :: "r"(0xaa55aa55UL));
asm(" mcr p15, 0, %0, c5, c0, 1\n" :: "r"(0xaa55aa55UL));
I have tried many permutations, with/without the final _DCACHE_INVALIDATE. I looked at the Cortex-A5-MPcore TRM and it seems that the Vybrid-A5 has no ACP or SCU active. The MQX code looks fine for flushing, although the L2 is a unified cache. I see the manual has some L1 cache debug registers. However, they take 'sets' and 'ways' as parameters. I have also tried to alter the MMU permissions to change the memory to 'device' so that it should be write-through, but I think that these are intended more for data only. I have also tried to disable the branch prediction, but I think this is cache related.
I think that the SDRAM is pre-populated with the routines during the soft boots, so some cache is setup with some latent routine that was copied via previous attempts to run the routine. I think the memory is almost '0xffffffff' after a hard reset. Is there any functional block that I have missed that I need to update to relocate and/or load code? Or source code examples I should look at? I have looked at the u-boot source and didn't see anything obvious. u-boot seems to work fine on hard resets; maybe MQX has enabled some extra functionality? This is on a Tower system. If I call the routines directly (without tz), then MQX will crash (or dabort loops forever). A soft reset and the direct calls to the relocated location are fine. If I call the routine at the original location as loaded by u-boot, then it executes always. With the tz, I have code to dump the contexts and I can see the 'PC' is set to the MQX abort_handler, with the abort lr set to the first instruction (+8), which seems to indicate the first code access fails.
A relocatable routines I use is below; I have many different implementations (using UART, SDRAM/iRAM, etc) and I don't think the issue is here, but I provide it for reference.
.align 8
.equ gpio0_base, 0x400ff000
ASM_PUBLIC(led_poll)
ASM_PUBLIC(led_poll_size)
ASM_PUBLIC_BEGIN(led_poll)
ASM_PUBLIC_FUNC(led_poll)
ASM_LABEL(led_poll)
movw r1, #:lower16:gpio0_base
movt r1, #:upper16:gpio0_base
mov r2, #24*2 @ 24 blinks.
1: mov r0, #(15<<22) @ gpio0-22 to 25.
str r0, [r1, #12] @ toggle leds.\
mov r0, #0x80000 @ spin loop delay.
2: subs r0, r0, #1
bne 2b
subs r2, r2, #1
bne 1b
bx lr
.ltorg
ASM_PUBLIC_END(led_poll)
led_poll_size: .word . - led_poll
Possibly, I can provide a binary; I would have to remove the tz support to give source.
EDIT: I retried with MQX 4.1 and the same issue seems to occur.
EDIT2: There appears to be some bugs in _a5_dcache_flush(). The shifts should not be hexadecimal and we should select the data cache with,
| MCR(15, 2, 0, 0, 0, 0); | /* Select data cache */ |
before looking at the sets/ways information. I still don't know if there are additional problems...