Code Warrior Library Project in MQX 4.2?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Code Warrior Library Project in MQX 4.2?

858 次查看
erictexley
Contributor I

In MQX4.1 there was a library project for CodeWarrior 10.x which would set up all the projects required to build MQX.   Does that project file exist in MQX4.2?  I don't see it

0 项奖励
回复
1 回复

749 次查看
danielchen
NXP TechSupport
NXP TechSupport

Hi Eric Texley

The library project files are in the relative build folders.

Let's take frdmK64f for example, the libraries are in the following folders

Freescale_MQX_4_2\mqx\build\cw10gcc\bsp_frdmk64f

Freescale_MQX_4_2\mqx\build\cw10gcc\psp_frdmk64f

Freescale_MQX_4_2\rtcs\build\cw10gcc\rtcs_frdmk64f

Freescale_MQX_4_2\mfs\build\cw10gcc\mfs_frdmk64f

I hope it helps

Have a great day!

Regards

Daniel

-----------------------------------------------------------------------------------------------------------

If this post answered your question, please click correct or helpful, thank you

0 项奖励
回复