Changing linker file for bootloader

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Changing linker file for bootloader

Jump to solution
2,580 Views
barbercolman
Contributor III

I have a MQX 3.7 and CW 10.1 I want to be able to bootloader. I edit the .lcf file and compile the project. If I exit and restart the project the linker file has reverted! How do I make a change to the linker perminate.

0 Kudos
Reply
1 Solution
1,903 Views
petr_uhlir
NXP Employee
NXP Employee

 

The original linker command file for Codewarrior is located in "\bsp\{board_name}\cw\" directory

After compilation of bsp library the linker file is copied by postbuild batch file "\build\bat\bsp_{board_name}.bat " to 

"\lib\{board_name}.cw10\bsp lib directory.

 

So if you have 2 options

1. Modify the original linker file

or

2. Change the Linker Command File path in your application project so it refers to your custom linker file.

   Menu->Project ->Properties->C/C++ Build->Settings->Tool Settings Tab->ARM Linker->Input->Linker Command File-> Browse...

You have to change it for all Build configurations or select [All configurations] in Build configuration settings.

 

 

View solution in original post

0 Kudos
Reply
4 Replies
1,904 Views
petr_uhlir
NXP Employee
NXP Employee

 

The original linker command file for Codewarrior is located in "\bsp\{board_name}\cw\" directory

After compilation of bsp library the linker file is copied by postbuild batch file "\build\bat\bsp_{board_name}.bat " to 

"\lib\{board_name}.cw10\bsp lib directory.

 

So if you have 2 options

1. Modify the original linker file

or

2. Change the Linker Command File path in your application project so it refers to your custom linker file.

   Menu->Project ->Properties->C/C++ Build->Settings->Tool Settings Tab->ARM Linker->Input->Linker Command File-> Browse...

You have to change it for all Build configurations or select [All configurations] in Build configuration settings.

 

 

0 Kudos
Reply
1,903 Views
barbercolman
Contributor III

Hi

I change the linker command file path for all confiurations. I also added my linker file to the linker files folder in the project. When I compiled I received a no rault toe make target for my linker config file. Any ideas?

0 Kudos
Reply
1,903 Views
DavidS
NXP Employee
NXP Employee

Hi Barber,

MQX is setup so that the RTOS gets built up with libraries that are placed in the mqx/libpath.

The application you build will link against those libraries.

When debugging an application the header files and linker files that get opened are in the mqx/lib path.  When the RTOS is built, the library and header files are copied from their source path to the mqx/lib path.  So any edits you make to a header file in the mqx/lib path will get over written the next time the RTOS is re-built (this has happened to me many times...).

So when editing a linker or header file, always check the path (mouse over the file name in the editor window).

Your method of placing the linker script into your project is OK too.

From your reply I do not understand the error you are getting.  Can you elaborate?

Regards,

David

0 Kudos
Reply
1,903 Views
barbercolman
Contributor III

Thanks it now makes more sense.

 

I a m new to Freescale and looking at the project in CW how do I tell which files can be edited? I see files that are linked and some of them can be edited and some can not! 

 

How do I know which is which

0 Kudos
Reply