Can't read directory from a separate task

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Can't read directory from a separate task

Jump to solution
3,075 Views
Stefan_75
Contributor II

Hi,

 

I'm using the ftp-usb example.

 

I'm trying to read the directory from the USB stick. Doing this with the code below, there's no problem. I'm using the code directly after installing the MFS in the USB_task.

 

Now, when I'm trying to read the directory periodically (e.g every minute) from a separate task i get a MQX_UNHANDLED_INTERRUPT at the ioctl command. All data needed to access the MFS at the USB stick are in a global struct (USB_st).

 

--- code start ----

 

sprintf (USB_st.filepath, "*.*");

 

USB_st.search.ATTRIBUTE = MFS_ATTR_READ_ONLY | MFS_ATTR_HIDDEN_FILE | MFS_ATTR_SYSTEM_FILE | MFS_ATTR_ARCHIVE;
USB_st.search.WILDCARD = USB_st.filepath;
USB_st.search.SEARCH_DATA_PTR = &USB_st.search_data;

 

USB_st.error_code_UL = ioctl(((USB_FILESYSTEM_STRUCT_PTR)(USB_st.usb_fs_handle->FS_FD_PTR)), IO_IOCTL_FIND_FIRST_FILE,(uint_32_ptr) &(USB_st.search));
while (USB_st.error_code_UL == MFS_NO_ERROR)
{
 USB_st.error_code_UL = _io_ioctl(USB_st.usb_fs_handle->FS_FD_PTR, IO_IOCTL_FIND_NEXT_FILE, (uint_32_ptr) &USB_st.search_data);
}

 

--- code end ----  

 

Anybody any idea? Thanks.

 

Stefan  

Labels (1)
Tags (1)
0 Kudos
Reply
1 Solution
1,298 Views
Stefan_75
Contributor II

Hi,

 

the data are in a struct like this:

 

--- code start --- 

 

typedef struct

{

      unit8   test;

      USB_FILESYSTEM_STRUCT_PTR    USB_fs_ptr;

 

}USB_ST;

 

USB_ST    Usb_st; 

 

 --- code end ---

 

The struct beginns at a adress, that is devidable through 4 (32 bit). When I'm trying to get "inner" adress from the USB_FILESYSTEM_STRUCT_PTR, the pointer to the adress begins at address that is devideable through 4 +1, becaus of the variable test.

 

Example:

 

values: 

test = 0xFF

Usb_st.USB_fs_ptr->FS_FD_PTR = 0x20001000

 

If you want to give Usb_st.USB_fs_ptr->FS_FD_PTR to the ioctl function:

 

ioctl(Usb_st.USB_fs_ptr->FS_FD_PTR, ..., ...) the function receive the adress 0xFF200010.

 

 

cu,

 

Stefan

View solution in original post

0 Kudos
Reply
1 Reply
1,299 Views
Stefan_75
Contributor II

Hi,

 

the data are in a struct like this:

 

--- code start --- 

 

typedef struct

{

      unit8   test;

      USB_FILESYSTEM_STRUCT_PTR    USB_fs_ptr;

 

}USB_ST;

 

USB_ST    Usb_st; 

 

 --- code end ---

 

The struct beginns at a adress, that is devidable through 4 (32 bit). When I'm trying to get "inner" adress from the USB_FILESYSTEM_STRUCT_PTR, the pointer to the adress begins at address that is devideable through 4 +1, becaus of the variable test.

 

Example:

 

values: 

test = 0xFF

Usb_st.USB_fs_ptr->FS_FD_PTR = 0x20001000

 

If you want to give Usb_st.USB_fs_ptr->FS_FD_PTR to the ioctl function:

 

ioctl(Usb_st.USB_fs_ptr->FS_FD_PTR, ..., ...) the function receive the adress 0xFF200010.

 

 

cu,

 

Stefan

0 Kudos
Reply