Can't display cpu usage or timeline

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Can't display cpu usage or timeline

3,142件の閲覧回数
kaiyueyang
Contributor III

    I'm using a K60FX512 MCU with MQX4.0 and CW10.4. I have created klog in my program. And I can see 'Performace data view' and 'stack usage'. But when I tried to open timeline, It tells me that 'no task switches found'. In cpu usage it shows nothing.

   I've tried both online and offline mode. Neither of them worked.

   I've used this in my last project which is on MQX3.8. And it just worked well. I don't know what's the difference.

タグ(2)
8 返答(返信)

2,289件の閲覧回数
Luis_Garabo
NXP TechSupport
NXP TechSupport

Hi Yang,

Since you already saw it working on MQX 3.8 I will assume you already added these two lines in the user_config.h file:

#define MQX_USE_LOGS                         1
#define MQX_KERNEL_LOGGING                   1

Make sure you recompiled PSP and BSP again after this change.

If so, then you need to check the example code I am attaching which I already tested and is showing with context switch timeline.


Regards,
Garabo

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信

2,289件の閲覧回数
kaiyueyang
Contributor III

Kernel log contains:

1. 0x00000000:37B91 -> FUN       _time_delay_ticks 0x0 0x0 0x0 0x0 0x0

2. 0x00000000:37F9B -> FUN            _sched_yield 0x1FFF1B9C 0x10002 0x2 0x1FFF21BC 0x0

3. 0x00000000:38393 -> FUN             _task_ready 0x1FFF1B9C 0x0 0x0 0x0 0x0

4. 0x00000000:3874E -> XFUN            _task_ready 0x0 0x0 0x0 0x0 0x0

5. 0x00000000:38C14 -> XFUN      _time_delay_ticks 0x0 0x0 0x0 0x0 0x0

6. 0x00000000:38FC8 -> FUN       _time_delay_ticks 0x5 0x0 0x0 0x0 0x0

7. 0x00000005:048E -> FUN             _task_ready 0x1FFF1B9C 0x0 0x0 0x0 0x0

8. 0x00000005:0865 -> XFUN            _task_ready 0x0 0x0 0x0 0x0 0x0

9. 0x00000005:0D97 -> XFUN      _time_delay_ticks 0x0 0x0 0x0 0x0 0x0

10. 0x00000005:1146 -> FUN       _time_delay_ticks 0xA 0x0 0x0 0x0 0x0

11. 0x0000000F:046A -> FUN             _task_ready 0x1FFF1B9C 0x0 0x0 0x0 0x0

12. 0x0000000F:0836 -> XFUN            _task_ready 0x0 0x0 0x0 0x0 0x0

13. 0x0000000F:0D5A -> XFUN      _time_delay_ticks 0x0 0x0 0x0 0x0 0x0

14. 0x0000000F:1117 -> FUN       _time_delay_ticks 0xF 0x0 0x0 0x0 0x0

15. 0x00000001E:0445 -> FUN             _task_ready 0x1FFF1B9C 0x0 0x0 0x0 0x0

16. 0x00000001E:081B -> XFUN            _task_ready 0x0 0x0 0x0 0x0 0x0

17. 0x00000001E:0D2C -> XFUN      _time_delay_ticks 0x0 0x0 0x0 0x0 0x0

18. 0x00000001E:10E6 -> FUN       _time_delay_ticks 0x14 0x0 0x0 0x0 0x0

19. 0x000000032:0461 -> FUN             _task_ready 0x1FFF1B9C 0x0 0x0 0x0 0x0

20. 0x000000032:0827 -> XFUN            _task_ready 0x0 0x0 0x0 0x0 0x0

21. 0x000000032:0D42 -> XFUN      _time_delay_ticks 0x0 0x0 0x0 0x0 0x0

22. 0x000000032:1109 -> FUN       _time_delay_ticks 0x19 0x0 0x0 0x0 0x0

23. 0x00000004B:045B -> FUN             _task_ready 0x1FFF1B9C 0x0 0x0 0x0 0x0

24. 0x00000004B:082D -> XFUN            _task_ready 0x0 0x0 0x0 0x0 0x0

25. 0x00000004B:0D48 -> XFUN      _time_delay_ticks 0x0 0x0 0x0 0x0 0x0

26. 0x00000004B:10F7 -> FUN       _time_delay_ticks 0x1E 0x0 0x0 0x0 0x0

27. 0x000000069:0455 -> FUN             _task_ready 0x1FFF1B9C 0x0 0x0 0x0 0x0

28. 0x000000069:0817 -> XFUN            _task_ready 0x0 0x0 0x0 0x0 0x0

29. 0x000000069:0D2B -> XFUN      _time_delay_ticks 0x0 0x0 0x0 0x0 0x0

30. 0x000000069:10EB -> FUN       _time_delay_ticks 0x23 0x0 0x0 0x0 0x0

31. 0x00000008C:0461 -> FUN             _task_ready 0x1FFF1B9C 0x0 0x0 0x0 0x0

32. 0x00000008C:083B -> XFUN            _task_ready 0x0 0x0 0x0 0x0 0x0

33. 0x00000008C:0D54 -> XFUN      _time_delay_ticks 0x0 0x0 0x0 0x0 0x0

34. 0x00000008C:1103 -> FUN       _time_delay_ticks 0x28 0x0 0x0 0x0 0x0

35. 0x0000000B4:045B -> FUN             _task_ready 0x1FFF1B9C 0x0 0x0 0x0 0x0

36. 0x0000000B4:0813 -> XFUN            _task_ready 0x0 0x0 0x0 0x0 0x0

37. 0x0000000B4:0D1C -> XFUN      _time_delay_ticks 0x0 0x0 0x0 0x0 0x0

38. 0x0000000B4:10D7 -> FUN       _time_delay_ticks 0x2D 0x0 0x0 0x0 0x0

39. 0x0000000E1:0442 -> FUN             _task_ready 0x1FFF1B9C 0x0 0x0 0x0 0x0

40. 0x0000000E1:0801 -> XFUN            _task_ready 0x0 0x0 0x0 0x0 0x0

41. 0x0000000E1:0D10 -> XFUN      _time_delay_ticks 0x0 0x0 0x0 0x0 0x0

42. 0x0000000E1:BC05 -> FUN          _taskq_suspend 0x1FFF174C 0x0 0x0 0x0 0x0

43. 0x0000000E7:73597 -> FUN           _taskq_resume 0x1FFF174C 0x1 0x0 0x0 0x0

44. 0x0000000E7:73AC4 -> FUN             _task_ready 0x1FFF1B9C 0x0 0x0 0x0 0x0

45. 0x0000000E7:73EA6 -> XFUN            _task_ready 0x0 0x0 0x0 0x0 0x0

46. 0x0000000E7:742C5 -> XFUN          _taskq_resume 0x0 0x0 0x0 0x0 0x0

47. 0x0000000E7:747D8 -> XFUN         _taskq_suspend 0x0 0x0 0x0 0x0 0x0

48. 0x0000000E7:8048B -> FUN          _taskq_suspend 0x1FFF174C 0x0 0x0 0x0 0x0

49. 0x0000000EE:51C55 -> FUN           _taskq_resume 0x1FFF174C 0x1 0x0 0x0 0x0

50. 0x0000000EE:52172 -> FUN             _task_ready 0x1FFF1B9C 0x0 0x0 0x0 0x0

51. 0x0000000EE:5253A -> XFUN            _task_ready 0x0 0x0 0x0 0x0 0x0

52. 0x0000000EE:52941 -> XFUN          _taskq_resume 0x0 0x0 0x0 0x0 0x0

53. 0x0000000EE:52E3A -> XFUN         _taskq_suspend 0x0 0x0 0x0 0x0 0x0

54. 0x0000000EE:5DE25 -> FUN          _taskq_suspend 0x1FFF174C 0x0 0x0 0x0 0x0

55. 0x0000000F5:30334 -> FUN           _taskq_resume 0x1FFF174C 0x1 0x0 0x0 0x0

56. 0x0000000F5:3081D -> FUN             _task_ready 0x1FFF1B9C 0x0 0x0 0x0 0x0

57. 0x0000000F5:30BF2 -> XFUN            _task_ready 0x0 0x0 0x0 0x0 0x0

58. 0x0000000F5:30FF9 -> XFUN          _taskq_resume 0x0 0x0 0x0 0x0 0x0

59. 0x0000000F5:314C2 -> XFUN         _taskq_suspend 0x0 0x0 0x0 0x0 0x0

60. 0x0000000F5:3A50F -> FUN          _taskq_suspend 0x1FFF174C 0x0 0x0 0x0 0x0

61. 0x0000000FC:EA10 -> FUN           _taskq_resume 0x1FFF174C 0x1 0x0 0x0 0x0

62. 0x0000000FC:EEE9 -> FUN             _task_ready 0x1FFF1B9C 0x0 0x0 0x0 0x0

63. 0x0000000FC:F2B0 -> XFUN            _task_ready 0x0 0x0 0x0 0x0 0x0

64. 0x0000000FC:F6B1 -> XFUN          _taskq_resume 0x0 0x0 0x0 0x0 0x0

65. 0x0000000FC:FB98 -> XFUN         _taskq_suspend 0x0 0x0 0x0 0x0 0x0

66. 0x0000000FC:1AEA5 -> FUN          _taskq_suspend 0x1FFF174C 0x0 0x0 0x0 0x0

67. 0x00000012:7F8A9 -> FUN           _taskq_resume 0x1FFF174C 0x1 0x0 0x0 0x0

68. 0x00000012:7FDE7 -> FUN             _task_ready 0x1FFF1B9C 0x0 0x0 0x0 0x0

69. 0x00000012:801B7 -> XFUN            _task_ready 0x0 0x0 0x0 0x0 0x0

70. 0x00000012:805BF -> XFUN          _taskq_resume 0x0 0x0 0x0 0x0 0x0

71. 0x00000012:80A8E -> XFUN         _taskq_suspend 0x0 0x0 0x0 0x0 0x0

72. 0x00000012:8BF93 -> FUN          _taskq_suspend 0x1FFF174C 0x0 0x0 0x0 0x0

73. 0x00000019:5DF91 -> FUN           _taskq_resume 0x1FFF174C 0x1 0x0 0x0 0x0

74. 0x00000019:5E49D -> FUN             _task_ready 0x1FFF1B9C 0x0 0x0 0x0 0x0

75. 0x00000019:5E85E -> XFUN            _task_ready 0x0 0x0 0x0 0x0 0x0

76. 0x00000019:5EC77 -> XFUN          _taskq_resume 0x0 0x0 0x0 0x0 0x0

77. 0x00000019:5F146 -> XFUN         _taskq_suspend 0x0 0x0 0x0 0x0 0x0

78. 0x00000019:6A9E1 -> FUN          _taskq_suspend 0x1FFF174C 0x0 0x0 0x0 0x0

79. 0x000000110:3C68B -> FUN           _taskq_resume 0x1FFF174C 0x1 0x0 0x0 0x0

80. 0x000000110:3CBA3 -> FUN             _task_ready 0x1FFF1B9C 0x0 0x0 0x0 0x0

81. 0x000000110:3CF64 -> XFUN            _task_ready 0x0 0x0 0x0 0x0 0x0

82. 0x000000110:3D37D -> XFUN          _taskq_resume 0x0 0x0 0x0 0x0 0x0

83. 0x000000110:3D87C -> XFUN         _taskq_suspend 0x0 0x0 0x0 0x0 0x0

84. 0x000000110:491EB -> FUN          _taskq_suspend 0x1FFF174C 0x0 0x0 0x0 0x0

85. 0x000000117:1AD7D -> FUN           _taskq_resume 0x1FFF174C 0x1 0x0 0x0 0x0

86. 0x000000117:1B2BD -> FUN             _task_ready 0x1FFF1B9C 0x0 0x0 0x0 0x0

87. 0x000000117:1B6A0 -> XFUN            _task_ready 0x0 0x0 0x0 0x0 0x0

88. 0x000000117:1BA95 -> XFUN          _taskq_resume 0x0 0x0 0x0 0x0 0x0

89. 0x000000117:1BF6A -> XFUN         _taskq_suspend 0x0 0x0 0x0 0x0 0x0

90. 0x000000117:27BE9 -> FUN          _taskq_suspend 0x1FFF174C 0x0 0x0 0x0 0x0

91. 0x00000011D:8BC06 -> FUN           _taskq_resume 0x1FFF174C 0x1 0x0 0x0 0x0

92. 0x00000011D:8C0E0 -> FUN             _task_ready 0x1FFF1B9C 0x0 0x0 0x0 0x0

93. 0x00000011D:8C4AC -> XFUN            _task_ready 0x0 0x0 0x0 0x0 0x0

94. 0x00000011D:8C8B3 -> XFUN          _taskq_resume 0x0 0x0 0x0 0x0 0x0

95. 0x00000011D:8CD82 -> XFUN         _taskq_suspend 0x0 0x0 0x0 0x0 0x0

96. 0x00000011E:6445 -> FUN          _taskq_suspend 0x1FFF174C 0x0 0x0 0x0 0x0

97. 0x000000124:6A2F1 -> FUN           _taskq_resume 0x1FFF174C 0x1 0x0 0x0 0x0

98. 0x000000124:6A819 -> FUN             _task_ready 0x1FFF1B9C 0x0 0x0 0x0 0x0

99. 0x000000124:6ABED -> XFUN            _task_ready 0x0 0x0 0x0 0x0 0x0

100. 0x000000124:6B007 -> XFUN          _taskq_resume 0x0 0x0 0x0 0x0 0x0

101. 0x000000124:6B500 -> XFUN         _taskq_suspend 0x0 0x0 0x0 0x0 0x0

102. 0x000000124:76CFF -> FUN          _taskq_suspend 0x1FFF174C 0x0 0x0 0x0 0x0

103. 0x00000012B:489A9 -> FUN           _taskq_resume 0x1FFF174C 0x1 0x0 0x0 0x0

104. 0x00000012B:48EC0 -> FUN             _task_ready 0x1FFF1B9C 0x0 0x0 0x0 0x0

105. 0x00000012B:49288 -> XFUN            _task_ready 0x0 0x0 0x0 0x0 0x0

106. 0x00000012B:49695 -> XFUN          _taskq_resume 0x0 0x0 0x0 0x0 0x0

107. 0x00000012B:49B70 -> XFUN         _taskq_suspend 0x0 0x0 0x0 0x0 0x0

108. 0x00000012B:54681 -> FUN          _taskq_suspend 0x1FFF174C 0x0 0x0 0x0 0x0

109. 0x000000132:270B5 -> FUN           _taskq_resume 0x1FFF174C 0x1 0x0 0x0 0x0

110. 0x000000132:275BD -> FUN             _task_ready 0x1FFF1B9C 0x0 0x0 0x0 0x0

111. 0x000000132:27988 -> XFUN            _task_ready 0x0 0x0 0x0 0x0 0x0

112. 0x000000132:27D89 -> XFUN          _taskq_resume 0x0 0x0 0x0 0x0 0x0

113. 0x000000132:2826A -> XFUN         _taskq_suspend 0x0 0x0 0x0 0x0 0x0

114. 0x000000132:31AF5 -> FUN          _taskq_suspend 0x1FFF174C 0x0 0x0 0x0 0x0

115. 0x000000139:577D -> FUN           _taskq_resume 0x1FFF174C 0x1 0x0 0x0 0x0

116. 0x000000139:5C85 -> FUN             _task_ready 0x1FFF1B9C 0x0 0x0 0x0 0x0

117. 0x000000139:606A -> XFUN            _task_ready 0x0 0x0 0x0 0x0 0x0

118. 0x000000139:6465 -> XFUN          _taskq_resume 0x0 0x0 0x0 0x0 0x0

119. 0x000000139:6940 -> XFUN         _taskq_suspend 0x0 0x0 0x0 0x0 0x0

120. 0x000000139:11DD9 -> FUN          _taskq_suspend 0x1FFF174C 0x0 0x0 0x0 0x0

121. 0x00000013F:7664E -> FUN           _taskq_resume 0x1FFF174C 0x1 0x0 0x0 0x0

122. 0x00000013F:76B47 -> FUN             _task_ready 0x1FFF1B9C 0x0 0x0 0x0 0x0

123. 0x00000013F:76F12 -> XFUN            _task_ready 0x0 0x0 0x0 0x0 0x0

124. 0x00000013F:77319 -> XFUN          _taskq_resume 0x0 0x0 0x0 0x0 0x0

125. 0x00000013F:77812 -> XFUN         _taskq_suspend 0x0 0x0 0x0 0x0 0x0

126. 0x00000013F:82C99 -> FUN          _taskq_suspend 0x1FFF174C 0x0 0x0 0x0 0x0

127. 0x000000146:54D2D -> FUN           _taskq_resume 0x1FFF174C 0x1 0x0 0x0 0x0

128. 0x000000146:55262 -> FUN             _task_ready 0x1FFF1B9C 0x0 0x0 0x0 0x0

129. 0x000000146:5563A -> XFUN            _task_ready 0x0 0x0 0x0 0x0 0x0

130. 0x000000146:55A5B -> XFUN          _taskq_resume 0x0 0x0 0x0 0x0 0x0

131. 0x000000146:55F48 -> XFUN         _taskq_suspend 0x0 0x0 0x0 0x0 0x0

132. 0x000000146:6177D -> FUN          _taskq_suspend 0x1FFF174C 0x0 0x0 0x0 0x0

133. 0x00000014D:33407 -> FUN           _taskq_resume 0x1FFF174C 0x1 0x0 0x0 0x0

134. 0x00000014D:3391A -> FUN             _task_ready 0x1FFF1B9C 0x0 0x0 0x0 0x0

135. 0x00000014D:33CF4 -> XFUN            _task_ready 0x0 0x0 0x0 0x0 0x0

136. 0x00000014D:3410D -> XFUN          _taskq_resume 0x0 0x0 0x0 0x0 0x0

137. 0x00000014D:3460C -> XFUN         _taskq_suspend 0x0 0x0 0x0 0x0 0x0

138. 0x00000014D:4009F -> FUN          _taskq_suspend 0x1FFF174C 0x0 0x0 0x0 0x0

139. 0x000000154:11AD6 -> FUN           _taskq_resume 0x1FFF174C 0x1 0x0 0x0 0x0

140. 0x000000154:11FD7 -> FUN             _task_ready 0x1FFF1B9C 0x0 0x0 0x0 0x0

141. 0x000000154:123B2 -> XFUN            _task_ready 0x0 0x0 0x0 0x0 0x0

142. 0x000000154:127B3 -> XFUN          _taskq_resume 0x0 0x0 0x0 0x0 0x0

143. 0x000000154:12CA2 -> XFUN         _taskq_suspend 0x0 0x0 0x0 0x0 0x0

144. 0x000000154:1E703 -> FUN          _taskq_suspend 0x1FFF174C 0x0 0x0 0x0 0x0

145. 0x00000015A:82990 -> FUN           _taskq_resume 0x1FFF174C 0x1 0x0 0x0 0x0

146. 0x00000015A:82E91 -> FUN             _task_ready 0x1FFF1B9C 0x0 0x0 0x0 0x0

This is what I get from serial terminal. It seems the log is normal?

0 件の賞賛
返信

2,289件の閲覧回数
Luis_Garabo
NXP TechSupport
NXP TechSupport

Send your user_config.h file please.


Regards,
Garabo

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信

2,289件の閲覧回数
kaiyueyang
Contributor III

/**HEADER**********************************************************************

*

* Copyright (c) 2008 Freescale Semiconductor;

* All Rights Reserved

*

*******************************************************************************

*

* THIS SOFTWARE IS PROVIDED BY FREESCALE "AS IS" AND ANY EXPRESSED OR

* IMPLIED WARRANTIES, INCLUDING, BUT NOT LIMITED TO, THE IMPLIED WARRANTIES

* OF MERCHANTABILITY AND FITNESS FOR A PARTICULAR PURPOSE ARE DISCLAIMED.

* IN NO EVENT SHALL FREESCALE OR ITS CONTRIBUTORS BE LIABLE FOR ANY DIRECT,

* INDIRECT, INCIDENTAL, SPECIAL, EXEMPLARY, OR CONSEQUENTIAL DAMAGES

* (INCLUDING, BUT NOT LIMITED TO, PROCUREMENT OF SUBSTITUTE GOODS OR

* SERVICES; LOSS OF USE, DATA, OR PROFITS; OR BUSINESS INTERRUPTION)

* HOWEVER CAUSED AND ON ANY THEORY OF LIABILITY, WHETHER IN CONTRACT,

* STRICT LIABILITY, OR TORT (INCLUDING NEGLIGENCE OR OTHERWISE) ARISING

* IN ANY WAY OUT OF THE USE OF THIS SOFTWARE, EVEN IF ADVISED OF

* THE POSSIBILITY OF SUCH DAMAGE.

*

*******************************************************************************

*

* $FileName: user_config.h$

* $Version : 3.8.4.0$

* $Date    : Sep-5-2012$

*

* Comments:

*

*   User configuration for MQX components

*

*END**************************************************************************/

#ifndef __user_config_h__

#define __user_config_h__

/* mandatory CPU identification */

#define MQX_CPU                 PSP_CPU_MK60DF120M

/* MGCT: <generated_code> */

#define BSPCFG_ENET_SRAM_BUF                      1

#define BSPCFG_ENABLE_I2C0                        0

#define BSPCFG_ENABLE_I2C1                        1

#define BSPCFG_ENABLE_II2C0                       0

#define BSPCFG_ENABLE_II2C1                       1

#define BSPCFG_ENABLE_SPI1                        1

#define BSPCFG_ENABLE_SPI2                        1

#define BSPCFG_ENABLE_FLASHX                      1

#define BSPCFG_ENABLE_IODEBUG                     0

#define BSPCFG_HAS_SRAM_POOL                      1

#define BSPCFG_ENABLE_TTYA                        0

#define BSPCFG_ENABLE_ITTYA                       1

#define BSPCFG_SCI0_BAUD_RATE                     19200

#define BSPCFG_ENABLE_TTYB                        0

#define BSPCFG_ENABLE_ITTYB                       1

#define BSPCFG_SCI1_BAUD_RATE                     19200

#define BSPCFG_ENABLE_TTYC                        0

#define BSPCFG_ENABLE_ITTYC                       1

#define BSPCFG_SCI2_BAUD_RATE                     19200

#define BSPCFG_ENABLE_TTYD                        0

#define BSPCFG_ENABLE_ITTYD                       1

#define BSPCFG_SCI3_BAUD_RATE                     19200

#define BSPCFG_ENABLE_TTYE                        0

#define BSPCFG_ENABLE_ITTYE                       1

#define BSPCFG_SCI4_BAUD_RATE                     19200

#define BSPCFG_ENABLE_TTYF                        0

#define BSPCFG_ENABLE_ITTYF                       1

#define BSPCFG_SCI5_BAUD_RATE                     19200

#define BSP_DEFAULT_IO_CHANNEL                    "ittyd:"

#define BSP_DEFAULT_IO_OPEN_MODE                  NULL

#define MQX_USE_IDLE_TASK                         1

#define MQX_USE_MUTEXES                           1

#define MQX_USE_LOGS                              1

#define MQX_TASK_DESTRUCTION                      1

#define MQX_KERNEL_LOGGING                        1

#define MQX_ENABLE_LOW_POWER                      0

#define RTCSCFG_ENABLE_ICMP                       1

#define RTCSCFG_ENABLE_SNMP                       0

#define RTCSCFG_ENABLE_UDP                        1

#define RTCSCFG_ENABLE_TCP                        1

#define RTCSCFG_ENABLE_STATS                      1

#define RTCSCFG_ENABLE_GATEWAYS                   1

#define FTPDCFG_USES_MFS                          1

#define TELNETDCFG_NOWAIT                         FALSE

#define HTTPDCFG_POLL_MODE                        0

#define HTTPDCFG_STATIC_TASKS                     0

#define HTTPDCFG_DYNAMIC_TASKS                    1

/* MGCT: </generated_code> */

/*

** include common settings

*/

/* use the rest of defaults from small-RAM-device profile */

#include "small_ram_config.h"

/* and enable verification checks in kernel */

#include "verif_enabled_config.h"

#endif /* __user_config_h__ */

0 件の賞賛
返信

2,289件の閲覧回数
Luis_Garabo
NXP TechSupport
NXP TechSupport

Hi Yang,

Yes, your file looks fine. It should be another problem. Could you please add a break point in the dispatch.S file just in the line where the context switch is being logged into the kernel log? Just in the same line like the screen shoot shows:

pastedImage_0.png

Once you reach that break point go and take a look to your KLOG in the task aware debugging (MQX menu)

Hope that helps to find what is the issue.


Regards,
Garabo

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

2,289件の閲覧回数
lfschrickte
Contributor IV

Have the same issue here. Activated both macros in the user_config.h file, recompiled and however can't even access kernel log via the MQX menu (as said in your reply). Can access, however, Stack Usage. CPU Usage View is also not working.

Using FRDM-K64F + MQX RTOS 4.1 + CW 10.6.

Thank you!

Luiz Fernando

0 件の賞賛
返信

2,289件の閲覧回数
Luis_Garabo
NXP TechSupport
NXP TechSupport

Hi Luiz,

I just tested with a few modifications to the previous code and adding a break point in the line 119. I am able to see the context switching and the CPU usage with no issues. I am attaching the new code tested in MQX 4.1 for FRDM-K64


Regards,
Garabo

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信

2,289件の閲覧回数
kaiyueyang
Contributor III

I've tried klog.c. It didn't work. The result is just the same as my own program.

0 件の賞賛
返信