Can I use the FNET V0.7.0 bootloader to my commercial projects?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

Can I use the FNET V0.7.0 bootloader to my commercial projects?

跳至解决方案
1,517 次查看
OOLife
Contributor III

 

Hi,

 

I want to know about FNET License policy.

 

That's hard to understand to me.

 

Can I use the FNET V0.7.0 bootloader to my commercial products or projects?

 

Could you guys explain about this more easily?

 

And, which is the best way to use FNET V0.7.0 legally with modification of FNET V0.7.0 ?

 

Thank you in advance

 

0 项奖励
回复
1 解答
840 次查看
butok
NXP Employee
NXP Employee

Hi,

 

 

>> Can I use the FNET V0.7.0 bootloader to my commercial products or projects?
Yes, you can.

The FNET code http://fnet.sourceforge.net/ is under the GNU Lesser General Public License
http://www.gnu.org/licenses/lgpl.html.
Briefly, it means that you can do with FNET what ever you want, you should NOT open your proprietary code.
The only obligation is, if you do changes in the FNET source codes (fixes, improvements rtc.), you should open them, make them available to community (or send directly to the FNET project).

 

Best regards,
Andrey Butok

在原帖中查看解决方案

0 项奖励
回复
1 回复
841 次查看
butok
NXP Employee
NXP Employee

Hi,

 

 

>> Can I use the FNET V0.7.0 bootloader to my commercial products or projects?
Yes, you can.

The FNET code http://fnet.sourceforge.net/ is under the GNU Lesser General Public License
http://www.gnu.org/licenses/lgpl.html.
Briefly, it means that you can do with FNET what ever you want, you should NOT open your proprietary code.
The only obligation is, if you do changes in the FNET source codes (fixes, improvements rtc.), you should open them, make them available to community (or send directly to the FNET project).

 

Best regards,
Andrey Butok

0 项奖励
回复