CW Licensing for MQX

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 
2,373件の閲覧回数
rdazcal
Contributor III

Greetings,

 

Is it possible to develop MQX applications using CodeWarior's special Edition? I mean, with the code size constrains and number of files constrains, will I have problems with it once my Evaluation License expires?

 

By development, I mean not only compilation but also flashing the board. (I'm using the Tower System with the MCF52259 MPU)

 

What about recompiling the BSP?

 

If the standard edition is not enough, which suite do I need?

 

Thank you

0 件の賞賛
返信
1 解決策
1,844件の閲覧回数
anthony_huereca
NXP Employee
NXP Employee

It is possible to use the Special Edition, but it will limit which applications and demos you can use.

 

You can look at this page in the lower left hand corner (click on "Example Applications and Labs") to see which projects, the ones with the astricks, will not work with Special Edition because of code size limitations. That is assuming the default MQX configuration settings, so you might be able to squeeze it down further with some tweaking of user_config.h.

 

The libraries, with the exception of the default RTCS library, should have no problems compiling. For RTCS, you might have to take out some features to get the library down to the 128K limit.

 

You should probably get a license that allows you to compile code for the amount of flash on the chip. So for the MCF52259, that would be 512k, which is the Basic edition. The list of CW versions and details can be found here: http://www.freescale.com/webapp/sps/site/overview.jsp?code=CW_SUITES&tid=CWH

 

Also note that the code size limitations differ based on which core you're using, so a ColdFire V2/V3/V4 has a different size limitaiton than a ColdFire V1 in the Special Edition.

 

Finally Task Aware Debugging is only enabled on the Professional version, so keep that in mind as well.

 

-Anthony

元の投稿で解決策を見る

0 件の賞賛
返信
3 返答(返信)
1,845件の閲覧回数
anthony_huereca
NXP Employee
NXP Employee

It is possible to use the Special Edition, but it will limit which applications and demos you can use.

 

You can look at this page in the lower left hand corner (click on "Example Applications and Labs") to see which projects, the ones with the astricks, will not work with Special Edition because of code size limitations. That is assuming the default MQX configuration settings, so you might be able to squeeze it down further with some tweaking of user_config.h.

 

The libraries, with the exception of the default RTCS library, should have no problems compiling. For RTCS, you might have to take out some features to get the library down to the 128K limit.

 

You should probably get a license that allows you to compile code for the amount of flash on the chip. So for the MCF52259, that would be 512k, which is the Basic edition. The list of CW versions and details can be found here: http://www.freescale.com/webapp/sps/site/overview.jsp?code=CW_SUITES&tid=CWH

 

Also note that the code size limitations differ based on which core you're using, so a ColdFire V2/V3/V4 has a different size limitaiton than a ColdFire V1 in the Special Edition.

 

Finally Task Aware Debugging is only enabled on the Professional version, so keep that in mind as well.

 

-Anthony

0 件の賞賛
返信
1,844件の閲覧回数
rdazcal
Contributor III

Thank you Anthony,

 

That was exactly the information I was looking for!

 

0 件の賞賛
返信
1,844件の閲覧回数
machinegeek
Contributor I
I recently purchased the MCF51CN in the Tower system and have the same concerns.
0 件の賞賛
返信