CMSIS DSP Library for Freescale compiler

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

CMSIS DSP Library for Freescale compiler

3,761 Views
shihab_thadathi
Contributor I

Hi

I want to use CMSIS DSP library functions for my MQX 4.0 project that works in TWRK70f120M using code_warrior IDE. I am able to use this functions for bareboard project using gcc compiler, but it shows Unknown compiler Error. Can i use cmsis dsp lib with freescale compiler?. Is there any document or guide describing  CMSIS lib porting for freescale compiler?.

Regards,

Shihab

0 Kudos
Reply
6 Replies

3,260 Views
ZhangJennie
NXP TechSupport
NXP TechSupport

hello Shihab,

please refer threads:

https://community.freescale.com/message/350214#350214

https://community.freescale.com/thread/324740

==============================

this answer is for you. if it helps, please click on "Correct Answer" button. thanks!

Best Regards,

ZhangJun

0 Kudos
Reply

3,260 Views
shihab_thadathi
Contributor I

Hi ZhangJennie ,


All of these links describe the use of CMSIS lib using gcc compiler. Is this possible with freescale compiler?



Thanks,

Shihab

0 Kudos
Reply

3,260 Views
ZhangJennie
NXP TechSupport
NXP TechSupport

Hi Shihab,

I have a CMSIS samples ever made under FSL compiler CW10.2. but it's around 30M. please send me your email address so that i can send it to you via transweb.

thanks!

==============================

this answer is for you. if it helps, please click on "Correct Answer" button. thanks!

Best Regards,

ZhangJun

3,260 Views
shihab_thadathi
Contributor I

Thanks ZhangJennie,


I have send you a message containing my email address.

0 Kudos
Reply

3,260 Views
ZhangJennie
NXP TechSupport
NXP TechSupport

Hi Shihab,

i just sent. the description of it is in SR 1-2924409127

==============================

this answer is for you. if it helps, please click on "Correct Answer" button. thanks!

Best Regards,

ZhangJun

0 Kudos
Reply

3,260 Views
shihab_thadathi
Contributor I

Thanks a lot ZhangJennie,


I will check this


Regards,

Shihab

0 Kudos
Reply