CGI interface related Query

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

CGI interface related Query

1,224 Views
utsavikalpesh
Contributor V

Hi,

I am using code warrior v10.2 and of MQX v4.0.

I am working on a project in which I need to communicate between Client(PC) and Server(Tower Module). I want to use CGI functionality to send or receive the data in server part.

But problem is my Client part (PC) is not a web page. It will be some king of utility that I have developed into Visual C++.

Now can I use CGI functionality that works without web pages??

As I have read that CGI is a script that is used to send the contents to web pages. Here in my case I want to send or receive the content to my Client Utility.Will CGI send the contents??

Please Help.

0 Kudos
Reply
1 Reply

1,124 Views
DavidS
NXP Employee
NXP Employee

Hi Utsavi,

Please look at appnote 4644 and how it implements client/server Discovery/Broadcast code to learn how they communicate.  It might work for your application.

AN4644, Remote Monitoring Solution Using MQX and Kinetis - Application Notes (REV 0)

20 Mar 2013 AN4644: This application note is intended to demonstrate the implementation  of a Remote Medical Monitor System using K53, K60, MED-EKG, and ...
  • PDF
  • 138KB
  • Application Notes: AN4644
Associated File: AN4644SW

Regards,

David

0 Kudos
Reply