CAN  initialization MK60DN512 + MQX

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

CAN  initialization MK60DN512 + MQX

855件の閲覧回数
profprogrammer
Contributor III

Hellow .

I need problem.

When I initialize a mail boxing 0 (ID 0x123) recive.

initialize a mail boxing 0 (ID 0x321) transmit/

data from the betraying MB[1] get to reception MB[0].

I not use interrupt.

I apply source codes. I use MQX drivers.

why are given from MB[1] I get to MB[0]?

how it is correct to initialize CAN?

Original Attachment has been moved to: mn.c.zip

Original Attachment has been moved to: chai.c.zip

0 件の賞賛
返信
1 返信

748件の閲覧回数
soledad
NXP Employee
NXP Employee

Hello Prof,

You can find an example code at the path C:\Freescale\Freescale_MQX_4_2\mqx\examples\can,

For boards twrk70f120m and twrk60n512 the new fsl_flexcan driver is used whereas for other boards including twrk20d72m, twrk21f120m, twrk40d100m, twrk40x256, twrk60 d100m, twrk60f120m, twrmcf52259, twrmcf54418, twrpxd10, twrpxn20, twrpxs30 the old kflexcan driver is used. You can use this example as reference.

Have a great day,
Sol

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信