Building MQX RTOS project using TWR-K60D100M on Codewarrior v10.6.4, Not able to build the Lib files (PSP) for the K60) controller

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Building MQX RTOS project using TWR-K60D100M on Codewarrior v10.6.4, Not able to build the Lib files (PSP) for the K60) controller

Jump to solution
1,643 Views
abhishekinamdar
Contributor II

     Hello, we are building the MQX RTOS project using the TWR - K60D100M on CodeWarrior v10.6.4 and FreesacleMQX on Windows 7, we are not able to Build Library file for the the board, its PSP for the K60D100M. Go through the following images for more details.

pastedImage_1.png

     Firstly, we tried to import and build the BSP, PSP, Shell file in to the work space, was able to build the following file into the Library folder as shown below.(PSP folder was not visible)

pastedImage_2.png

    

     When we started programming with the new project, following errors where observed. Please go through the images and do the needful to resolve this errors.

pastedImage_4.png

Regards

Abhishek

Labels (1)
0 Kudos
Reply
1 Solution
1,521 Views
soledad
NXP Employee
NXP Employee

Hello Abhishek,

Please check the attached video.


Have a great day,
Sol

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

View solution in original post

0 Kudos
Reply
2 Replies
1,522 Views
soledad
NXP Employee
NXP Employee

Hello Abhishek,

Please check the attached video.


Have a great day,
Sol

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply
1,521 Views
DavidS
NXP Employee
NXP Employee

Hi Abhishek,

MQX_4.2 has different/new method for opening projects.

Please review the following PDF document in your MQX_4.2 installation path.

C:/Freescale/Freescale_MQX_4_2/doc/tools/cw/MQX_CW10_Getting_Started.pdf

Please let us know if you need further help.

Regards,

David

0 Kudos
Reply