Bug report: MQX 4.1 Linux build scripts.

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Bug report: MQX 4.1 Linux build scripts.

1,456 Views
billpringlemeir
Contributor V

All of the master Linux builds scripts use the following idiom,

$(cd path && ./build_gcc_arm.sh nopause)

The $() are not needed.  This is like $(echo ls).  Ie, the output of the commands (stdout) will be run as a command.  The lines should only be,

cd path && ./build_gcc_arm.sh nopause
Tags (3)
0 Kudos
Reply
1 Reply

1,306 Views
soledad
NXP Employee
NXP Employee

Hi Bill,

It is always helpfully to receive customer’s feedback, thank you for your comment.


Have a great day,
Sol

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------