Bootloader_vybrid project built on DS-5 studio, Error : unable to open sdcard driver

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Bootloader_vybrid project built on DS-5 studio, Error : unable to open sdcard driver

1,343件の閲覧回数
manjug
Contributor III

I have built the bootloader_vybrid example project for MQX for target Tower_VF65GS10_A5 core.I have prepared SDCARD according to readme file provided in project folder and copied the bootloader binary to sdcard and also my application binary image and a5 initialisation file to sdcard. when i inserted sdcard and powered bootloader is running but following error is seen and halted below is the log messages from terminal : 

Bootloader from A5 as primary core, dual core

======================

Mounting filesystem

Error : unable to open sdcard driver 

why it is not able open sdcard driver eventhough its has opened sdhc driver and installed sdcard driver please help me.....

ラベル(1)
0 件の賞賛
返信
0 返答(返信)