Best current WIFI solution for MQX

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Best current WIFI solution for MQX

ソリューションへジャンプ
2,660件の閲覧回数
oscargarciaabad
Contributor III

Hi all,

I'm wondering which is the current state of WIFI in MQX. I need a module which is able to use MQX TCP/IP stack ( and it has an already developed MQX driver). I need the following features:

- SoftAP

- IPv4

- IPv6

- Fully certified.

I'm using MQX 4.1 and a TWR-K60. I saw that the modules from gainspan, redpine an atheros are not longer supported and are not recommended for futute designs. I also saw the module TWR-LTRX-XPWK but I don't know whether is an MQX driver for it.

Could anybody guide me on this proces?

Thank you,

Oscar.

ラベル(1)
0 件の賞賛
返信
1 解決策
2,353件の閲覧回数
danielchen
NXP TechSupport
NXP TechSupport

Hi Oscar:

I think the best solution for MQX+WIFI is Atheros.

Regarding the TWR-LTRX-XPWK, you can ask the provider


Have a nice day,
Daniel

元の投稿で解決策を見る

0 件の賞賛
返信
3 返答(返信)
2,354件の閲覧回数
danielchen
NXP TechSupport
NXP TechSupport

Hi Oscar:

I think the best solution for MQX+WIFI is Atheros.

Regarding the TWR-LTRX-XPWK, you can ask the provider


Have a nice day,
Daniel

0 件の賞賛
返信
2,353件の閲覧回数
oscargarciaabad
Contributor III

Hi Daniel,

Thanks for your answer. I'm a little concerned about this:

"This development board is no longer in production and not recommended for future design"

Regards,

Oscar

0 件の賞賛
返信
2,353件の閲覧回数
thiagow
Contributor III

What is the recommended design now?

0 件の賞賛
返信